Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Difficulties using NTP with a GPS + Raspberry Pi (HELP!)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 2854 views
  • Users 0 members are here
  • raspberry_pi
Related

Difficulties using NTP with a GPS + Raspberry Pi (HELP!)

vk3pb
vk3pb over 13 years ago

Hi all

 

I have been asking around for help on other forums with this problem but noone has come up with a solution thus far. I hope that someone out there can help.

 

I am trying to get my model B pi to work with a bu-353 GPS. I have achieved some success but I can't get ntp to automatically fetch the time on boot.

 

I followed the instructions here

 

http://blog.retep.org/2012/06/18/getting-gps-to-work-on-a-raspberry-pi/

 

but found that I needed to make a few modifications to get cgps working

 

Here's what I did

 

sudo apt-get install gpsd gpsd-clients python-gps

 

I then ran

 

sudo dpkg-reconfigure /etc/gpsd

 

to set gpsd to automatically boot. I added -n in the options but didn't put in  /dev/ttyUSB0 as the port but rather left it to automatically find the USB plug.

 

I then manually edited GPSD and added in

 

chmod a+rw /dev/ttyUSB0

 

The reason for these two tweaks is that the gps was not loading up properly and cgps -s just waited a few seconds and went back to the command line. The tweaks seem to have fixed that.

 

Now if I start my pi and then put in the comamnd line

 

cgps -s

 

I can see what the gps is seeing, location information sats etc all in text format. If I run xgps I can see a graphical version of this. This works every time although can take a coupel of seconds to get a fix.

 

So far so good.

 

Per the web page I now proceed to try and set up ntp

 

sudo apt-get install ntp

Installation is probably unnecessary as ntp is already installed.

 

Now I go to the /etc directory and sudo nano ntp.conf and add in the following lines

 

# gps ntp
server 127.127.28.0 minpoll 4
fudge  127.127.28.0 time1 0.183 refid NMEA
server 127.127.28.1 minpoll 4 prefer
fudge  127.127.28.1 refid PPS

 

and then type

 

sudo service ntp restart

 

Ntp restarts. cgps-s continues to work ok but my time does not update like it should. Although I can get a fix on satellites and can see the time in cgps it doesn;t get picked up by NTP like it should.

 

How can I get NTP to load up the time from satellites at boot properly with the above setup? I would be grateful for some help as I am a beginner at Linux and I think a lot of people out there would like to know how to set up a cheap gps like this with the Pi.

 

Thanking you

  

Peter

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    It's been a while since I wrote that original blog post & there have been some who have reported problems depending on what GPS unit they are using.

     

    One issue has been the existing examples available online on setting this up.

     

    Someone did say about PPS & USB. One person did say that with a minor mod on some units you can get PPS running - I've not had any spare time to investigate that but even then with USB it wouldn't be as accutate as a native serial port.

     

    I've come across gpstime recently as well after someone commented about it http://blog.retep.org/2012/06/18/getting-gps-to-work-on-a-raspberry-pi/#comment-988 again a lack of time recently has meant I've not tried it yet.

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    It's been a while since I wrote that original blog post & there have been some who have reported problems depending on what GPS unit they are using.

     

    One issue has been the existing examples available online on setting this up.

     

    Someone did say about PPS & USB. One person did say that with a minor mod on some units you can get PPS running - I've not had any spare time to investigate that but even then with USB it wouldn't be as accutate as a native serial port.

     

    I've come across gpstime recently as well after someone commented about it http://blog.retep.org/2012/06/18/getting-gps-to-work-on-a-raspberry-pi/#comment-988 again a lack of time recently has meant I've not tried it yet.

     

    Peter