Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Data Acquisition System for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 706 subscribers
  • Views 1248 views
  • Users 0 members are here
  • analog_to_digital
  • raspberry_pi
  • raspberrypi
  • audio_interface
Related

Data Acquisition System for the Raspberry Pi

e14 Contributor
e14 Contributor over 13 years ago

In the last year, we've been impressed by the Raspberry Pi.  We believe that its capabilities and price point are a world changer.

 

We would like to bring to market, a flexible, low-cost ($35) data acquisition system for the Raspberry Pi.   Our system brings an 8 channel, 200 ksps, 10 bit analog to digital converter to the platform.  Notable hardware features include a programmable voltage reference, and user selectable AC or DC coupling.  There are several software solutions available to acquire data, including a java based (multi-platform - Windows, Linux, Mac OS) Remote Scope Application, a Remote Spectrum Application, as well as command line applications to take measurements.

 

We think that the Raspberry Pi combined with the RAS-DAS-1 provides a low-cost way for students to conduct experiments and put the fun back into science and math.  Towards that end, we are introducing an accessory card for the data acquisition system geared towards capturing audio data.  It is called the Audio explorer, and includes 4 electret microphones (with the accompanying high-gain amplifiers), and audio input jacks to easily bring audio data into the RAS-DAS-1 and the Raspberry Pi.

 

With this system, students can perform science experiments such as measuring the speed of sound, use trigonometry to determine the direction a sound comes from, or determine how far away a wall might be by listening for echoes (using a type of sonar).

 

We are introducing a kickstarter campaign to bring this technology to market, and would appreciate any assistance you might provide in spreading the word.

 

http://www.kickstarter.com/projects/254558907/data-acquisition-system-for-raspberry-pi

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Perhaps wattminder instruments need to communicate this in a better way.

     

    The purpose of this product is to provide general purpose analog data acquisition to the Raspberry Pi at a good price / value.  It is intended for people who do not want to build their own board, and want to use a powerful computer like the raspberry pi to get data and  process it.

     

    The price for the data acquisition card is $35 (the same price as the raspberry pi).  (The $50K is the target goal in order to go to production, and have the boards made in quantitty - fabricated, assembled, tested, etc.).

     

    The system is more than just an ADC chip.  It is a system which provides a programmable reference voltage (as well as other sources for VREF), AC/DC coupling capability, input protection circuitry, external power inputs (so that you could provide a quiet power supply to it), an a utility op-amp with gains of 1x, 2x, 4x, and 8x.

     

    All of this is in the same form factor as the Raspberry Pi.

     

    There is also software which grabs data across a network and plots it (which makes it like a hackable oscilloscope).   (Since the software is all within the raspberry pi environment, this makes debugging much easier than for instance connecting up an arduino nano, and a raspberry pi, and debugging between the two).

     

    The enclosure is a different story.  I think it's quite an elegant looking device, which is composed of a top an bottom with easy access to the raspberry pi via the sides.  The open sides provide lots of ventilation.  The enclosure provides space for 2-3 cards, and can be expanded as needed.

     

    When it comes down it, value is in the eye of the beholder.  Chips themselves are just sand and plastic, with a lot of processing.  This system provides value for those who don't want to bother with making their own boards, soldering surface mount chips, testing/debugging (i.e.: dealing with solder shorts, etc.), as well as providing everything in a neat package.

     

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Perhaps wattminder instruments need to communicate this in a better way.

     

    The purpose of this product is to provide general purpose analog data acquisition to the Raspberry Pi at a good price / value.  It is intended for people who do not want to build their own board, and want to use a powerful computer like the raspberry pi to get data and  process it.

     

    The price for the data acquisition card is $35 (the same price as the raspberry pi).  (The $50K is the target goal in order to go to production, and have the boards made in quantitty - fabricated, assembled, tested, etc.).

     

    The system is more than just an ADC chip.  It is a system which provides a programmable reference voltage (as well as other sources for VREF), AC/DC coupling capability, input protection circuitry, external power inputs (so that you could provide a quiet power supply to it), an a utility op-amp with gains of 1x, 2x, 4x, and 8x.

     

    All of this is in the same form factor as the Raspberry Pi.

     

    There is also software which grabs data across a network and plots it (which makes it like a hackable oscilloscope).   (Since the software is all within the raspberry pi environment, this makes debugging much easier than for instance connecting up an arduino nano, and a raspberry pi, and debugging between the two).

     

    The enclosure is a different story.  I think it's quite an elegant looking device, which is composed of a top an bottom with easy access to the raspberry pi via the sides.  The open sides provide lots of ventilation.  The enclosure provides space for 2-3 cards, and can be expanded as needed.

     

    When it comes down it, value is in the eye of the beholder.  Chips themselves are just sand and plastic, with a lot of processing.  This system provides value for those who don't want to bother with making their own boards, soldering surface mount chips, testing/debugging (i.e.: dealing with solder shorts, etc.), as well as providing everything in a neat package.

     

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor

    @Tony,

     

    Prompted by your posting I had a look at Wattminder's website - they don't publish a schematic but from the picture of the board I'm even less enthusiastic. They make  a big thing about audio but the basic data acquisition system is just no good for audio. A variable voltage reference and variable gain (not clear if adjustable per channel by software) is just no substitute for using an adc designed for audio (16 bits or more, standard sampling rates, simultaneous sampling, anti-aliasing filters) . As I mentioned earlier such adcs are cheap enough.

     

    A company looking for $50k investment should have a product that's a bit more state of the art.

     

    MK