Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problems HDMI to VGA
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 968 views
  • Users 0 members are here
  • raspberry_pi
Related

Problems HDMI to VGA

e14 Contributor
e14 Contributor over 13 years ago

I have a Raspberry pi, model B, 512.  

No problems at all when I connected the HDMI port to a friend's HD TV.

 

I bought a used Sony VGA monitor, manufactured in 2004 - MODEL SDM HS73.

This works perfectly when connected to the VGA port on my laptop. 

 

I bought from MCM Electronics: "PiView HDMI to VGA converter for the Raspberry Pi - Exclusively from element14", quoting from the package.

 

When I connected the Sony monitor to my Rpi via the PIView I get the message

"OUT OF RANGE

RESOLUTION > 1280 X 1024"

on the monitor.

 

Looking up the specifications for the monitor I read:  "Native Resolution 1280 x 1024"

 

Which device -- the Rpi or the PiView -- is asking for the out-of-range resolution?

If the PiView is responsible,  should I return it?

If the Rpi is to blame, what will fix it?

 

In the meantime, I have ordered a HDMI to VGA converter with its own power supply.

 

Any help will be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • tthomas
    tthomas over 13 years ago

    I'm thinking your problem is the monitor.  I have used PiView on several monitors without a proble.  On the other hand the maximun resolution I have seen on a standard TV used as a monitor has been 1360X760

    I use as a development station two 32 inch TVs set to their max res.  Had problems getting it to work until I reloadsed the video driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to tthomas

    Thanks for the help.  Sorry I took so long to get back.  I played around with 'config.txt'  and after a while I got it to work after a fashion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    What did you do to your script to get things to work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    What did you do to your script to get things to work?