Raspberry Pi Forum PI FACE cant import module into Python
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 676 subscribers
  • Views 2252 views
  • Users 0 members are here
  • piface_digital
  • raspberry_pi
Related

PI FACE cant import module into Python

Former Member
Former Member over 12 years ago

Hello

Can anybody help me get piface module imported into Python.

Having followed the instructions in the element 14 guide.

I have edited raspt-blacklist.conf and added the # infront of the blacklist spi-bcm2708

Install of software seemed to go OK and the piface graphical emulator works fine.

 

The problem is that when we open IDLE3 or IDLE and

 

import piface.pfio

 

we get an error saying ImportError: No module named piface.pfio

 

Can anyone help me?

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 12 years ago

    Are you sure that the piface directory with all the stuff has been created in your home directory?

    I think there is an error in the install.txt script that you are told to download by the PiFace documentation.

    (wget http://oi.cs.man.ac.uk/download/install.txt)

    Open the file with an editor (like nano) and change the line

    pushd ~/

    to

    pushd   (i.e. remove the ~/ ).

    Now execute the wget http://oi.cs.man.ac.uk/download/install.txt  and check if the piface directory has been created.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ratbag3366
    ratbag3366 over 12 years ago in reply to Former Member

    I too have the same problem. I have tried twice - from the ground up with a clean installation of the latest Raspbian (and updates) then followed the install process to the letter. Bizzarely the piface emulator works - leds come on, relays switch etc. Try to to the "import piface.pfio as" and you get the "ImportError: No Module named piface.pfio".

     

    I'm at a loss as what to do now...

     

    I have even manually ensure that the various scripts did what they were supposed to e.g. add pi to the spi groups etc.

     

    Weird.

     

    Can anyone help please?

     

    Update:

     

    Ah Ha!

     

    I tried running the ~/piface/python/test/piface_test.py script (as sudo) and it worked. I did a ls -l on the file and it was owner:root group:root so i chown and chgrp my effort to the same and ran it (as sudo) and it worked!!!!!!!!!!!

     

    Yahoo...

     

    Now - how to fix this so that I can run everything as user pi? because I edited the priveledges I can no longer use IDLE3 to edit the file (i now must use sudo vi).

     

    Ok - the "ImportError: No module name piface.pfio" is permissions related - so how to fix...

     

    ?

     

    Help appreciated.

     

    Further Update:

     

    I resistalled Raspbian from scratch + updates.

    Ran the installation process - thinking I may have run it as sudo last time(s).

     

    Same problem - won't load but will if i change to chown my file.py to root.

     

    This is dumb - is this happening to anyone else?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to ratbag3366

    Try this:

    in the install.txt file replace

    pushd ~/

    by this:

    pushd

     

    Cheers,  Francis

     

    Quoting ratbag3366 <messages@element14.com>:

     

    Andrew Harwood 

    http://www.element14.com/community/people/ratbag3366 created the 

    discussion

     

    "Re: PI FACE cant import module into Python"

     

    To view the discussion, visit: 

    http://www.element14.com/community/message/76232#76232/l/re-pi-face-cant-import-module-into-python

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to Former Member

    I am very new to this, only getting my Pi and Piface last week, so I applogise if my thoughts are incorrect.

     

    I have the same problem. "ImportError: No Module named piface.pfio" when trying to use IDLE3 or IDLE

     

    However if I create some simple test code for the PiFace Board and run my test program directly through TerminalTX by changing the directory to Pi/PiFace/Python/Test  ie (python MyTest.py) then it works correctly, so I assume the piface profile can be loaded from where ever 'Python' calls it using TerminalTX in the code source directory.

     

    So I guess it must be some kind of path issue when trying to run the code using IDLE3 as it will use a different directory location which my not have access to the piface.pfio

     

    I also changed the install.txt as above from pushd ~/ to pushd, restarted my Pi but still same problem, should I re-download the software package PiFace Software (wget http://pi cs.man ac.uk/download/install.txt) and then run the 'hash install.txt' again OR just re-run the 'hash install.txt again with the modified install.txt.

     

    If anyone has any thoughts as to what the problem is then I would be very greatfull.

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago

    Still playing with the Pi and trying to get PiFace to work with python shell.

     

    Just as a update, I re-installed from the begining again with a clean SD card and I can now import the piface profile in IDLE, but not in IDLE3, I assume IDLE3 does not import due to some kind of path or it could be a diffrent syntax as I have noticed that the print command is diffrent between IDLE and IDLE3.

     

    I have had ago with scrach, but I am a bit stuch with this MESH function to share varibles as I can not make a MESH Connection between Piface and Scratch. I will keep trying and if I get it working I will update the post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago

    Hi I am having the import problem ... did you ever get piface to work in python?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ratbag3366
    ratbag3366 over 12 years ago in reply to Former Member

    Nope - My enthusiasm with raspberry has wained. Partly because of this issue but also due to the fact that I would like to drive a screen but can't, and that when it comes to running python, there are ample tools on Mac/Windows that allow you to both programme and run Python (including a cool Pythonista app for iPAD/iPhone) a lost faster than the Raspberry. Also the final straw is that on a weekly basis my SD card would get corrupted and i'd have to set up from scratch - got board with that…

     

    Other than driving a motor or a few LED's I haven't used it much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to ratbag3366

    Both my pi and piface work fine so I am sure there is some way you could

    fix whatever problem you have

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • piface
    piface over 12 years ago

    Latest PiFace code is included in Raspbian by default. Packages, code and instructions are available from:

    https://github.com/piface/pifacedigitalio

     

    Edit: For those looking for installation instructions, visit http://www.piface.org.uk/guides/Install_PiFace_Software/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago

    Hi All,

     

    After spending several days (image - Documents that come with the PiFace say "get started with the PiFace ... in less than 10 minutes", ... ah!) I found a number of problems.

     

    I'm running Raspbrian Linux version 3.10.25+, the Linux version number can be found by typing "uname -r" at the command line.  The instructions that are delivered with the PiFace seem to be for a version that is much earlier and are useless. You get the error saying "ImportError: No module named piface.pfio". Andrew Robinson's suggestion of using http://piface.github.io/pifacedigitalio/installation.html... almost gets you there but is missing one step.

     

    I found that you need to enable the SPIT interface on http://www.piface.org.uk/guides/Install_PiFace_Software/Enabling_SPI/

     

    You do this by:

     

        

    PiFace products need the SPI pins on the Raspberry Pi to be enabled in order to function, this is simple enough to do. To enable the SPI, you must update to the latest version of the raspi-config tool, so open a Terminal and use the command

    sudo apt-get install raspi-config

    and enter Y when required.

    Now start raspi-config by typing

    sudo raspi-config

    To view the list of advanced configuration options, select Option 8 Advanced Options.

    Choose the A5 SPI option. Set this to "Yes"

    Select "Ok" then "Finish"

     

    Happliness is watching that LED flash for the first time...good luck.

     

    Cheers

     

    Muzz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.