Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help with wiring piface to an L298 h bridge
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 707 subscribers
  • Views 1047 views
  • Users 0 members are here
  • raspberry_pi
  • piface
Related

Help with wiring piface to an L298 h bridge

e14 Contributor
e14 Contributor over 13 years ago

I have a Pi-Face which I have successfully used to switch on and off some LED's but I'm a bit stuck on taking the next step - to drive a robot chassis.

I purchased one of these l298 motor drivers but I'm completely stuck on how to connect up the pi faces open collector outputs to the l298.

From searching about on the net it appears that it definitely possible but I just cant figure it out.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    Problemchild over 13 years ago

    Taking a look at the Ebay link I see it has seperate power and enable links etc.

    to test I would connect the motor to the output then power the  motor supply.

    The built in Regulator will supply the  5V for the logic.

    If the motor supply is less than 7V then you will need to supply the 5V externally as the regulator needs at least 2 V to opperate well

     

    Don't bother to connect to the pi try setting the inputs to the correct logic level by connecting them to GND or 5V and see if you get your

    desired result if not then your program logic is at fault and you best take another look at the L"(* datasheet and the truth table in it .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 13 years ago

    Taking a look at the Ebay link I see it has seperate power and enable links etc.

    to test I would connect the motor to the output then power the  motor supply.

    The built in Regulator will supply the  5V for the logic.

    If the motor supply is less than 7V then you will need to supply the 5V externally as the regulator needs at least 2 V to opperate well

     

    Don't bother to connect to the pi try setting the inputs to the correct logic level by connecting them to GND or 5V and see if you get your

    desired result if not then your program logic is at fault and you best take another look at the L"(* datasheet and the truth table in it .