Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum After School club projects
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 706 subscribers
  • Views 3499 views
  • Users 0 members are here
  • raspberry_pi
  • school
  • eduction
Related

After School club projects

GreenYamo
GreenYamo over 13 years ago

Hello, Hopefully within the next couple of weeks I'll be helping out in a local school's Pi club.

The format is pretty much free form, about an hour or so after school.

 

I'd love some ideas from this group as to what would be a good project for an hour or so - it can be anything, a Python Project, some GPIO interfacing, Scratch.

 

The Teaching and Learning Resources topic on the foundation's forum only has just over 300 posts, I was hoping for a bit more than that !

 

Thank you.

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    I'm about on the same page, trying to figure some projects that are not just programming and can be "pre packaged" for a ~45 minute or less session.

     

    We are starting rolling with the Geekbus from Geekdom, the idea is to go to middle schools and high schools (10-15 years age group) and have kids arrive in groups for about 45 minutes and have a hand on experience with electronics, computer science, networking, etc.

     

    Right now we have some simple projects with Arduino, but the time we have is so limited that we have the projects almost pre-wired and the kids only need to add few connections to the Arduino board, power and load and run the sketch for the project.

     

    We are now putting together some project with simple Lego Mindstorm projects.

     

    I've been struggling to find something interesting and easy to setup and quick to put together but with a Raspberry Pi, now that the Model A is becoming available in the US, if we are able to power it with a WiFi dongle included so we can use the same Netbooks we use for the Arduinos as a power source and console via vnc, that will be a plus since we won't have to deal with extra setup to provide power to the Rpis (we have two generators on the bus.

     

    We are also planning some summer camps at Geekdom where we'll have more time and better space to setup stuff, so we can go for more complex projects, I found that the project that Drew showed during the webinar about driving a stepper motor from Scratch could be an interesting and cool experience for the kids.

     

    I'll share whatever we learn putting this stuff together.

     

    Cheers

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 13 years ago

    I'm about on the same page, trying to figure some projects that are not just programming and can be "pre packaged" for a ~45 minute or less session.

     

    We are starting rolling with the Geekbus from Geekdom, the idea is to go to middle schools and high schools (10-15 years age group) and have kids arrive in groups for about 45 minutes and have a hand on experience with electronics, computer science, networking, etc.

     

    Right now we have some simple projects with Arduino, but the time we have is so limited that we have the projects almost pre-wired and the kids only need to add few connections to the Arduino board, power and load and run the sketch for the project.

     

    We are now putting together some project with simple Lego Mindstorm projects.

     

    I've been struggling to find something interesting and easy to setup and quick to put together but with a Raspberry Pi, now that the Model A is becoming available in the US, if we are able to power it with a WiFi dongle included so we can use the same Netbooks we use for the Arduinos as a power source and console via vnc, that will be a plus since we won't have to deal with extra setup to provide power to the Rpis (we have two generators on the bus.

     

    We are also planning some summer camps at Geekdom where we'll have more time and better space to setup stuff, so we can go for more complex projects, I found that the project that Drew showed during the webinar about driving a stepper motor from Scratch could be an interesting and cool experience for the kids.

     

    I'll share whatever we learn putting this stuff together.

     

    Cheers

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    > ... but the time we have is so limited that we have the projects almost pre-wired and the kids only need to add few connections to the Arduino board, power and load and run the sketch for the project.

     

    I suppose any exposure to electronics is a good thing, but it frightens me to see

    such limited exposure hyped as a meaningful learning experience.  I can't think

    of any other skill, whether it be learning a sport, or a musical instrument, or

    a foreign language, or an academic subject, where a single 45-minute exposure

    is so hyped.

     

    I am reminded of Little Jack Horner, who stuck in his thumb, pulled out a plum,

    and thought he was really cool, when he wasn't.

     

    > We are also planning some summer camps at Geekdom where we'll have more time and better space to setup stuff, ...

     

    I like that plan a lot better.

     

    There's something in particular that rubs me the wrong way about handing a

    beginner a complicated program and suggesting that they try to modify it,

    on the theory that software maintenance is something that can be done by

    rank beginners, without any programming skill and without any understanding

    of how the program works.

     

    Yes, you can find where it says "green" and change that to "blue", and

    maybe that will have the desired effect.  And yes, there is a certain amount

    of trial-and-error involved in real-world programming, particularly in maintaining

    someone else's code.  But the goal in programming is to understand what

    you're doing, not just thrash around until the program seems to work.