Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54326 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hello everybody, newbie here. Well newbie to the Pi/Beagle/Arduino/RT Linux world, not to embedded software engineering generally - cut my teeth on embedded 8086/ASM-86/PLM-86/iRMX systems 25 years ago, have written many a line of heavily multithreaded C/C++ on embedded and server systems, and have enjoyed knocking out the odd dual-6502 system for educational purposes. Ah those were the days, before we all got sucked into PC programming.

     

     

    But I'm rusty and looking to have some fun with ARM.

     

    So...my 2 cents on this discussion:

     

    Some say you should pick the best hardware/OS for the individual job at hand, and favour using a dedicated CPU for hardware interfaces. 

     

    However I prefer to pick one (reasonably priced) board for all the projects I have in mind. I don't want to have to learn and support multiple board personalities, idiosyncrasies and programming/operating environments. I can accept that that will sometimes mean shoe-horning a square board peg into a round application hole. Nobody has argued that angle.

     

    In my search for such a board I've discounted RPi (weak ISA, too many idiosyncrasies) and, sadly, also BBB due to its pathetic video (apparently it isn't considered 'cool' here to have media/video applications in mind, but I do).

     

    A real contender (albeit at double the cost) seems to be this. I wondered if the dedicated back end microcontroller advocates have seen that and have opinions.

     

    I could settle for BBB if there were ever likely to be:

     

    1) a "proper HDMI" shield, ie. providing 1080p with h/w acceleration for H264 etc.  

     

    2) a coprocessor shield, such that either the BBB or shield could be the front end hard RT coprocessor with the other one being the application processor.

     

    As long as said shields cost less than the base BBB board. Given that an RPi Model A (=$25 as is) could do the functionality, that seems like a reasonable ask. An RPi-A shield, anyone?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Hi Chris,

     

    By video, do you mean still images, or video playback (i.e. H.264 and other codecs), or 3D rendering (e.g. computer animation)? For stills the BBB I think can achieve full HD (the 1024x1028 is a software limitation in some images - the BBB is still a very new product). For video playback, it's hard to say - I've not seen good performance with Youtube (I see many frames dropped) but possibly the libraries are not making use of the acceleration features today. H.264 ought to be possible. For 3D rendering, I've not had a chance to try out the 3D processor built-in (it's not something that currently interests me). But, I think I agree that overall for full HD, the RPI is more suited.

     

    However, embedded apps may not require full HD.

    For embedded apps with video, it is also possible to connect to LCD panels directly (the parallel video bus is brought out to pins on the connector) with the BBB. It allows cheap LCDs from handheld games/smartphones to be used.

    For desktop apps, RPI is preferable, since it has full HD capability today - with the caveat that performance is low for running performance intensive apps. Still, it could be useful for kiosk style uses.

    Regarding the Udoo device that you mention - I'm pretty familiar with some of the Atmel SAM family members (and I like them), however they do run at a slower speed than the PRU devices, and therefore you may end up still requiring additional hardware like a CPLD anyway. The PRUs are simpler than the SAM devices, and are useful for high speed interfacing (and there are two of them), but they also integrate extremely well to the main processor - no need for an API, so you get high-speed interfacing using shared memory. Apparently there is work going on to create an API too.

     

    For battery-powered use-cases (likely in many embedded apps) the BBB is ideal too - it has a built in Li-Ion battery charger.

     

    If the requirement is small, there are lots of lower cost Atmel boards, or a FRDM board, and for more powerful use-cases I'm currently using the BBB. For other use-cases I'm currently using servers :-)

     

    The Udoo looks great too, but I'm just not ready for it - if I needed the additional capability of a SAM co-processor, I would personally add it using a tiny daughter card, at very low cost. There are also CPLD add-ons for the RPI for example (See Guzunty Pi). Also, at the cost of the Udoo, I couldn't have them in some applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    You're almost tempting me into creating a huge table with boards on columns and  features required by specific applications on rows.  It should be enough to use 0-9 as rough estimates of degree of support provided by each board, coresponding cell colouring from red for 0 to green for 9 (low saturation to keep the numbers visible), and a final expandible row and column for board notes and app notes respectively.

     

    App areas and features are more numerous than embedded boards with application processors, so this is probably the right way around.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    You're almost tempting me into creating a huge table with boards on columns and  features required by specific applications on rows.  It should be enough to use 0-9 as rough estimates of degree of support provided by each board, coresponding cell colouring from red for 0 to green for 9 (low saturation to keep the numbers visible), and a final expandible row and column for board notes and app notes respectively.

     

    App areas and features are more numerous than embedded boards with application processors, so this is probably the right way around.