Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54162 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    gdstew over 13 years ago

    I'd like to add another pro for the BeagleBoard Black.

     

    With the exceptions of the integer real time processors PRU-ICSS (not sure at this point why that is), and the PowerVR GPU for

    well known reasons, the AM3359 technical documentation from TI is excellent to the point of overwhelming. The Technical Reference

    Manual is over 4000 pages. No I did not accidentally add any zeros !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    With the exceptions of the integer real time processors PRU-ICSS (not sure at this point why that is), and the PowerVR GPU for well known reasons, the AM3359 technical documentation from TI is excellent to the point of overwhelming.

     

    You're right about the proprietary GPU, that seems to be an endemic problem for open source in the industry.  It's not true for the PRU-ICSS though.

     

    The PRU-ICSS is fully documented in the Technical Reference Manual SPRUH73C, with the entirety of chapter 4 (250 pages) devoted to it.  Also, there is a full package of PRU-related materials on Github, including more documentation and source code of the PRU's PASM assembler, a Linux loader, demos, etc.  I've even checked that the assembler compiles and it does.

     

    The BeagleBone materials on Github are at https://github.com/beagleboard/am335x_pru_package

     

    The PRU has been used successfully in quite a number of projects as a quick web search shows, and this long predates the BeagleBone Black since the original BeagleBone uses a slightly different version of the same AM3359 SoC.

     

    Morgaine.

     

    Addendum: Repeating the link to TI's wiki pages on PRU which I gave in my first post on this thread, in case it was missed when looking for docs.  There is a developers' link at the bottom of that first page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to jamodio

    I agree with you - there really isn't much of a price difference when you factor in no SD card or power supply is required.  The out of box experience is quite nice.  You simply connect the BB Black via USB cable to your computer.  It appears as a mass-storage device with a start html page.  Opening that takes you through a tutorial. 

     

    The BB Black also creates a virtual Ethernet network over USB cable, so the HTML-based tutorial can communicate with BB Black.  Right off the bat, you can edit BoneScript (Javascript for BeagleBone) in the starter tutorial page and that code will run on the Bone. 

     

    For a fuller experience, you can also click the link to open the Cloud9 IDE.  All that without any need for power supply, SD card, Ethernet cable, WiFi adapter or serial cable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to fustini

    I agree with you, Drew and jamodio.

     

    Superior experience for beginners out of the box, superior experience for experts later, with far more extensive hardware interfacing potential, the programming of PRUSS, and the creation and stacking of capes.  We were talking about a simple comparison table between Pi and BBB, but I don't think that's likely to indicate just how much more advanced the BBB experience and potential really is.

     

    The Pi is a nice little gadget if your application can work within its limits and foibles, and it has no same-price challengers yet as a home media center.  What's more, Pi Model A has no directly comparable challengers on price at all.  However, the Pi's range of "Best for application X" has now been reduced very sharply by BBB.  And somewhat embarassingly, BBB has much more education potential than Pi, and most of the Pi educational examples will work just as well or better on BeagleBones because they are typically generic Linux applications.

     

    This is a great time to be involved with ARM, so many excellent choices. image

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    PSoC has had limited success, largely because the chips have been rather expensive.  PSoC4 is supposed to change this by providing a highly capable SoC for US$1.

     

    Did you notice that the  CY8CKIT-042 PSoC4 Pioneer Kit board contains, in addition to the PSoC4 target device, a PSoC5 device that's used for board programming and debug?  (The intro video mentioned it.)  If PSoC4 is the cheap device, you'd think they'd use a second PSoC4 to provide that function on this cheap board.

     

    It seems a little bizarre, but I guess they already had PSoC5 code developed for the required function, and don't expect to sell enough boards to recoup additional development required to use the cheaper part instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    John Beetem wrote:

     

    PSoC has had limited success, largely because the chips have been rather expensive.  PSoC4 is supposed to change this by providing a highly capable SoC for US$1.

     

    Did you notice that the  CY8CKIT-042 PSoC4 Pioneer Kit board contains, in addition to the PSoC4 target device, a PSoC5 device that's used for board programming and debug?  (The intro video mentioned it.)  If PSoC4 is the cheap device, you'd think they'd use a second PSoC4 to provide that function on this cheap board.

     

    It seems a little bizarre, but I guess they already had PSoC5 code developed for the required function, and don't expect to sell enough boards to recoup additional development required to use the cheaper part instead.

    Yes, I saw that.  It's not at all unusual to have a much more capable part as the program/debug interface.  If I've read the data sheets correctly, the PSoC4 only has 32KB flash and 4KB SRAM, while the PSoC5 has 256KB flash and 64KB SRAM.  It's hard to squeeze much into 32K+4KB, particularly if the code is written by people who didn't grow up carrying around boxes of punched cards (2000 cards per box * one box per arm * two arms per human = 4000 lines of code that you can "comfortably" carry around if you have two arms).

     

    Reminds me of an LPXpresso board I have for the LPC1114FBD48/301,1LPC1114FBD48/301,1 -- a Cortex-M0 with 32KB flash and 4-8 KB RAM.  It's controlled by an LPC3154 -- an ARM9 with 192KB RAM.  I don't know how this compares to an mbed because my mbed has the controller's part number erased.

     

    It's often the case that the control SoC is the one to play with, provided that the vendor hasn't disabled access.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Reminds me of an LPXpresso board I have for the LPC1114FBD48/301,1LPC1114FBD48/301,1 -- a Cortex-M0 with 32KB flash and 4-8 KB RAM.  It's controlled by an LPC3154 -- an ARM9 with 192KB RAM.

     

    Haha.  That's a pretty severe case of an application processor in servitude to a microcontroller.  It can't be impressed. image

     

    I guess it's only a matter of time before Cortex-A series devices are given such roles too, particularly if a small realtime microcontroller needs a full-function IPv6 stack and comprehensive networking apps, and the simplest way of providing this is by giving it an entire Linux subsystem on a different SoC.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I guess it's only a matter of time before Cortex-A series devices are given such roles too, particularly if a small realtime microcontroller needs a full-function IPv6 stack and comprehensive networking apps, and the simplest way of providing this is by giving it an entire Linux subsystem on a different SoC.

    Actually, at some point it might be a good idea just to have the vendor's eval board be a BeagleBone cape.  That way they don't have to design their own controller hardware.  One problem with this is that the vendor has to worry about whether the user has a compatible operating system.  I don't have experience with Linux device drivers, but it may also be that it's a lot easier to write the whole debug controller on a bare chip than to write the Linux driver image  Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

     

    How is any ARM SOC with a proprietary GPU considered to be open hardware ? Isn't that a contradiction of terms ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    John Beetem wrote:

     

    Note that I didn't mention RasPi -- the vendor needs an open hardware project so it's not stuck if the controller board is discontinued.

     

    How is any ARM SOC with a proprietary GPU considered to be open hardware ? Isn't that a contradiction of terms ?

    Well, technically you're right since open source hardware (OSH) requires that all chips be fully documented.  However, my example of using BeagleBone as the controller for a chip's demo board doesn't need the GPU so for this application BeagleBone is indeed OSH.  You have open schematics, everything documented except GPU (I personally believe the PRUSS omission in latest TRM is an oversight), Gerbers, BOM, and all chips can be purchased in low volumes.  This is very different from RasPi, where most of the SoC is undocumented and it cannot be purchased in low volumes, and there are no Gerbers.

     

    I don't know what discussion OSH advocates are having about GPUs.  I suspect some argue that if you provide a GPU + binary blob, then as long as the API interface is fully documented you can think of the GPU as an OpenGL black box that happens to be implemented with downloadable black-box microcode.  However, in that case I would say you can't call it a GPU -- it's an embedded OpenGL engine where the implementation is hidden the same way you don't expose the innards of the ARM implementation.  IMO if you call it a GPU, then you have to let me program it or it's not OSH.

     

    I find the fact that FPGA bit streams are undocumented is much more annoying.  Yet, OSH champions like FPGAs since it lets them design their own open CPU architectures.  So plenty of opportunities to argue about how many angels can dance on the head of a pin.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Well, technically you're right since open source hardware (OSH) requires that all chips be fully documented.  However, my example of using BeagleBone as the controller for a chip's demo board doesn't need the GPU so for this application BeagleBone is indeed OSH. 

    There's no argument that GPU's are a problem and are likely to remain locked up behind a wall of patents, cross licensing and whatnot. So regardless of other issues the Pi isn't on the same playing field here. Most other SoCs are an Arm core with an undocumented, propriatary, GPU along for the ride, you can ignore the GPU, probably even turn it off and still use the rest of the SoC. For the Pi, you have an undocumented, propriatary Videocore GPU, with an Arm along for the ride - you can't get to the Arm without the GPU as the SoC is first and foremost a GPU.

    Even if the interface into that black box was fully documented it doesn't matter. A patent or licensing dispute could render you unable to legally use the GPU firmware and so unable to access the Arm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to johnbeetem

    Another advantage for the BeagleBone Black, beyond OSHW, is that the BeagleBoard.org development community (TI employees, Linux kernel maintainers & various individuals) have been working hard to get all remaining patches accepted by the mainline.  jkridner has told me that is an important goal for the project to be able to just git clone Linus's kernel and go.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 13 years ago in reply to johnbeetem

    Another advantage for the BeagleBone Black, beyond OSHW, is that the BeagleBoard.org development community (TI employees, Linux kernel maintainers & various individuals) have been working hard to get all remaining patches accepted by the mainline.  jkridner has told me that is an important goal for the project to be able to just git clone Linus's kernel and go.