Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    mynameisJim wrote:

     

    http://www.raspberrypi.org/wp-content/uploads/2012/02/BCM2835-ARM-Peripherals.pdf

     

    John could you expound on how this is less than what TI did?  It seems like the same level of information on both sides with the main hold out being both their GPU info. 

    I'll do a quick compare with the AM335X TRM rev C, which is the one I have handy.

     

    The first clue is the number of pages: BCM = 205, TI = 4593.

     

    USB: BCM has reference to a Synopsys document, which I think you have to register with Synopsys to download.  Even then I'm not sure it's available or useful.  TI has 1612 pages on USB.

     

    Interrupts: BCM has 10 pages, not sure if it covers what you need to write an OS.  TI has 200 pages.  Don't know if this is just because TI is more versatile, or whether it covers more ground.

     

    System initialization and booting: BCM has 0 pages, TI has 60.  This is something you need to know to write an OS or do bare-metal programming.  BCM actually boots using the GPU, so totally closed.

     

    Chip pinout: not in BCM documents, present in TI AM335X data sheet.  Ditto for detailed pin electrical information, such as absolute max voltages.

     

    As Billy has said upstream, most people don't need this information.  RasPi is indended for end users who will use it as a programming tool, so the information given is adequate.  Beagles are intended for serious development, with Bone intended for "makers" who need lots of I/O.  Some people have done bare-metal programming with RasPi, and it's possible by treating the GPU's "binary blob" as a closed boot ROM.  However, if I'm doing bare-metal programming, I really want to understand what I'm doing and I want the level of documentation provided by TI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    mynameisJim wrote:

     

    http://www.raspberrypi.org/wp-content/uploads/2012/02/BCM2835-ARM-Peripherals.pdf

     

    John could you expound on how this is less than what TI did?  It seems like the same level of information on both sides with the main hold out being both their GPU info. 

    I'll do a quick compare with the AM335X TRM rev C, which is the one I have handy.

     

    The first clue is the number of pages: BCM = 205, TI = 4593.

     

    USB: BCM has reference to a Synopsys document, which I think you have to register with Synopsys to download.  Even then I'm not sure it's available or useful.  TI has 1612 pages on USB.

     

    Interrupts: BCM has 10 pages, not sure if it covers what you need to write an OS.  TI has 200 pages.  Don't know if this is just because TI is more versatile, or whether it covers more ground.

     

    System initialization and booting: BCM has 0 pages, TI has 60.  This is something you need to know to write an OS or do bare-metal programming.  BCM actually boots using the GPU, so totally closed.

     

    Chip pinout: not in BCM documents, present in TI AM335X data sheet.  Ditto for detailed pin electrical information, such as absolute max voltages.

     

    As Billy has said upstream, most people don't need this information.  RasPi is indended for end users who will use it as a programming tool, so the information given is adequate.  Beagles are intended for serious development, with Bone intended for "makers" who need lots of I/O.  Some people have done bare-metal programming with RasPi, and it's possible by treating the GPU's "binary blob" as a closed boot ROM.  However, if I'm doing bare-metal programming, I really want to understand what I'm doing and I want the level of documentation provided by TI.