Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    Billy Thornton wrote:

     

    Getting stuff out of synopsys is like getting blood out of a stone. But since the number of people who can write decent USB code is pretty small its not a great loss!

    Thank you for confirming my suspicion about Synopsys.  Regarding whether or not it's a loss, I would suggest that we can't expect good USB code without good USB hardware documentation.

     

    Out of interest, if the boot sequence results in a machine ready to run baremetal code, why do you need information about it? You can drive the arm as much as you like from that point onwards. All you need that information for is to write a bootloader, which you already have...my readin of the baremetal forum (not my interest so I didnt do a lot of readin) is that its all going pretty well. If you want to do it you can, the docs are not particularly limiting.

    As with any closed source code, if there's anything wrong with it you can't fix it.  It was this frustration that led RMS to the Four Freedoms.  In the RasPi case, it's apparently working out OK for bare-metal programmers but I'm not following the bare-metal forum either so I don't know if they're exposing problems that require "binary blob" fixes.

     

    Personally, I prefer having the flexibility of knowing what my boot code is doing.  Maybe this comes from memorizing the PDP-8 RIM loader at an impressionable age, and knowing what it did in assembly and machine language.  Having this kind of access lets me do unusual things, like the time I booted an IBM PPC403GA embedded PowerPC through a FIFO.  That was a challenge, because a FIFO can only execute sequential code -- you can't branch.  Having full control of the machine language was necessary in that case.  Besides, it gives me Isaac Asimov's "Feeling of Power", which makes computing in general more enjoyable IMO.

     

    And why do you need chip pinouts? You've got the header pinouts which is where it all happens. No one can buy the chip, so no need of the pinouts.

    I simply included this as part of the differences between BCM and TI documentation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    Billy Thornton wrote:

     

    Getting stuff out of synopsys is like getting blood out of a stone. But since the number of people who can write decent USB code is pretty small its not a great loss!

    Thank you for confirming my suspicion about Synopsys.  Regarding whether or not it's a loss, I would suggest that we can't expect good USB code without good USB hardware documentation.

     

    Out of interest, if the boot sequence results in a machine ready to run baremetal code, why do you need information about it? You can drive the arm as much as you like from that point onwards. All you need that information for is to write a bootloader, which you already have...my readin of the baremetal forum (not my interest so I didnt do a lot of readin) is that its all going pretty well. If you want to do it you can, the docs are not particularly limiting.

    As with any closed source code, if there's anything wrong with it you can't fix it.  It was this frustration that led RMS to the Four Freedoms.  In the RasPi case, it's apparently working out OK for bare-metal programmers but I'm not following the bare-metal forum either so I don't know if they're exposing problems that require "binary blob" fixes.

     

    Personally, I prefer having the flexibility of knowing what my boot code is doing.  Maybe this comes from memorizing the PDP-8 RIM loader at an impressionable age, and knowing what it did in assembly and machine language.  Having this kind of access lets me do unusual things, like the time I booted an IBM PPC403GA embedded PowerPC through a FIFO.  That was a challenge, because a FIFO can only execute sequential code -- you can't branch.  Having full control of the machine language was necessary in that case.  Besides, it gives me Isaac Asimov's "Feeling of Power", which makes computing in general more enjoyable IMO.

     

    And why do you need chip pinouts? You've got the header pinouts which is where it all happens. No one can buy the chip, so no need of the pinouts.

    I simply included this as part of the differences between BCM and TI documentation.