Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    John Beetem wrote:

     

    As with any closed source code, if there's anything wrong with it you can't fix it.  It was this frustration that led RMS to the Four Freedoms.  In the RasPi case, it's apparently working out OK for bare-metal programmers but I'm not following the bare-metal forum either so I don't know if they're exposing problems that require "binary blob" fixes.

    Various problems have arisen over time that can only be fixed in the GPU blob. JamesH in particular seems to often dismiss these things with something along the lines of "the gpu binary is closed so nobody can help apart from rpf/broadcom and we're all too busy to look" and seems to combine that with an attitude of the broadcom engineers being the smartest people on the planet and it being impossible for anyone else to be smart enough to help anyway, which I find rather condescending if not outright arrogant.

     

    Interestingly, in a thread about the camera, 'gsh' at least hints at having discussions with Broadcom to allow the CSI peripheral details to be added to the arm datasheet. Seemingly to allow others to remove the roadblock of the gpu being the only thing that can talk to the camera/csi and the lack of resource from Broadcom/RPF to do things to the gpu blob.

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=24660&p=346189&hilit=CSI+peripheral&sid=7c21f71bcdec17f98913be74a083680c#p346189

    Whether that will ever actually come to anything is anyone's guess, but as at least some sort of acknowledgment that the binary blob can't/won't do everything and that there needs to be other ways it seems significant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    John Beetem wrote:

     

    As with any closed source code, if there's anything wrong with it you can't fix it.  It was this frustration that led RMS to the Four Freedoms.  In the RasPi case, it's apparently working out OK for bare-metal programmers but I'm not following the bare-metal forum either so I don't know if they're exposing problems that require "binary blob" fixes.

    Various problems have arisen over time that can only be fixed in the GPU blob. JamesH in particular seems to often dismiss these things with something along the lines of "the gpu binary is closed so nobody can help apart from rpf/broadcom and we're all too busy to look" and seems to combine that with an attitude of the broadcom engineers being the smartest people on the planet and it being impossible for anyone else to be smart enough to help anyway, which I find rather condescending if not outright arrogant.

     

    Interestingly, in a thread about the camera, 'gsh' at least hints at having discussions with Broadcom to allow the CSI peripheral details to be added to the arm datasheet. Seemingly to allow others to remove the roadblock of the gpu being the only thing that can talk to the camera/csi and the lack of resource from Broadcom/RPF to do things to the gpu blob.

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=24660&p=346189&hilit=CSI+peripheral&sid=7c21f71bcdec17f98913be74a083680c#p346189

    Whether that will ever actually come to anything is anyone's guess, but as at least some sort of acknowledgment that the binary blob can't/won't do everything and that there needs to be other ways it seems significant.