Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Billy Thornton wrote:

     

    I thoughthe camera attached straight to the gpu?

    That's what we've been told.

    How woudl the arm talk to the camera if ists actually connected to the gpu?

     

    Well that's something we don't know, but may find out in time. 

     

    Consider this, we know that both eth GPU and Arm can talk to the sdcard since the GPU loads code from there before the Arm is given access, we know both the Arm and GPU can access the same i2c channels using the same peripherals - various problems with interactions between the camera and the other channel show this http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=46594&p=367156sid=cf5e12c4e01c81e4484db4a56595cb99#p367156   http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=46299&p=367991&sid=cbfc64ff58b4d45d1b7f489ff0bb0686#p367991  we don't know the internal details, but it seems fair to assume that both the GPU and the Arm have access to all the same peripherals.  However, if that is the case then we only know how to access the ones they've documented for the Arm, there may be other things in the SoC that the Arm can talk to that we simply don't know exist.

     

    The way gsh replied to that thread certainly suggests that the arm can talk to the csi peripheral and that it's simply a matter of getting that documented.  Whether it's any easier to get docs out of broadcom or synopsys I have no idea. Whether what gsh implies in his reply is true or not I have no way of knowing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Billy Thornton wrote:

     

    I thoughthe camera attached straight to the gpu?

    That's what we've been told.

    How woudl the arm talk to the camera if ists actually connected to the gpu?

     

    Well that's something we don't know, but may find out in time. 

     

    Consider this, we know that both eth GPU and Arm can talk to the sdcard since the GPU loads code from there before the Arm is given access, we know both the Arm and GPU can access the same i2c channels using the same peripherals - various problems with interactions between the camera and the other channel show this http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=46594&p=367156sid=cf5e12c4e01c81e4484db4a56595cb99#p367156   http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=46299&p=367991&sid=cbfc64ff58b4d45d1b7f489ff0bb0686#p367991  we don't know the internal details, but it seems fair to assume that both the GPU and the Arm have access to all the same peripherals.  However, if that is the case then we only know how to access the ones they've documented for the Arm, there may be other things in the SoC that the Arm can talk to that we simply don't know exist.

     

    The way gsh replied to that thread certainly suggests that the arm can talk to the csi peripheral and that it's simply a matter of getting that documented.  Whether it's any easier to get docs out of broadcom or synopsys I have no idea. Whether what gsh implies in his reply is true or not I have no way of knowing.