Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    My redux from the last few exchanges is that Pi is seen as a vehicle for the initial stages of  engineering education (which of course is true, and very welcome), but owing to the various areas in which the board and SoC are closed, it's not a vehicle for medium or advanced engineering education.  The complex bits are restricted to just a privileged few.  Not ideal, but you can't win them all.

     

    It's a pity though --- it didn't have to be so.  Whatever the obstacles, where there is a will there is always a way, and if the will were there, the whole thing could have been made open hardware.  Or, more optimistically, can still be made fully open hardware some time in the future.  Full disclosure rights to so-called "proprietary IP" can be purchased --- it just requires sufficient will to allocate funds to it, aided by good negotiating skills to convince the design rights holder that their horrible USB design core isn't worth much anyway.

     

    Even the VideoCore will in time become obsolete and superceded by something better.  How about planning for that time, and getting ready to acquire full disclosure rights to it?  Where there is will there is always a way.

    This follows a bit what I was just saying.  Whenever the foundation released more information, the overwhelming response was negativity that they weren't making it more opened rather than positive praise for the work they were accomplishing on the open source front.  Personally, I look for the point at which a device becomes effectively completely open sourced.  Take the USB stack like we've been discussing.  There might be a handful of individuals who actually want to dig into making their own USB driver even fewer who want to mess with the GPU at a lower level than the 4 or 5 interfaces that have been opened up from the ARM side of things.

     

    I guess what I'm trying to say is that we need more of a weighted average when it comes to talking about how open a board is and we need to be more ready to praise when anyone gets additional documentation released instead of our default response of "stop be proud about only getting this much".  I definitely need to do some more research into how the bone lets you work with the GPU, but it seems like in terms of openness they both fall short in the same GPU location.  The pi might be slightly more open in that you can do more tweaks via the config.txt file, though from our current definition we'd probably rank the Bone as more open for obscuring the GPU.  sigh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    My redux from the last few exchanges is that Pi is seen as a vehicle for the initial stages of  engineering education (which of course is true, and very welcome), but owing to the various areas in which the board and SoC are closed, it's not a vehicle for medium or advanced engineering education.  The complex bits are restricted to just a privileged few.  Not ideal, but you can't win them all.

     

    It's a pity though --- it didn't have to be so.  Whatever the obstacles, where there is a will there is always a way, and if the will were there, the whole thing could have been made open hardware.  Or, more optimistically, can still be made fully open hardware some time in the future.  Full disclosure rights to so-called "proprietary IP" can be purchased --- it just requires sufficient will to allocate funds to it, aided by good negotiating skills to convince the design rights holder that their horrible USB design core isn't worth much anyway.

     

    Even the VideoCore will in time become obsolete and superceded by something better.  How about planning for that time, and getting ready to acquire full disclosure rights to it?  Where there is will there is always a way.

    This follows a bit what I was just saying.  Whenever the foundation released more information, the overwhelming response was negativity that they weren't making it more opened rather than positive praise for the work they were accomplishing on the open source front.  Personally, I look for the point at which a device becomes effectively completely open sourced.  Take the USB stack like we've been discussing.  There might be a handful of individuals who actually want to dig into making their own USB driver even fewer who want to mess with the GPU at a lower level than the 4 or 5 interfaces that have been opened up from the ARM side of things.

     

    I guess what I'm trying to say is that we need more of a weighted average when it comes to talking about how open a board is and we need to be more ready to praise when anyone gets additional documentation released instead of our default response of "stop be proud about only getting this much".  I definitely need to do some more research into how the bone lets you work with the GPU, but it seems like in terms of openness they both fall short in the same GPU location.  The pi might be slightly more open in that you can do more tweaks via the config.txt file, though from our current definition we'd probably rank the Bone as more open for obscuring the GPU.  sigh.