Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

     

    The current definitions we're working with are flawed as they encourage manufactures to put more info where we can't touch it

     

    You're confusing two things:  being more open, and having more functionality.  They're completely and utterly different concepts.

     

    Sure, those who want to use advanced but closed functions will praise their availability, but this has absolutely nothing to do with the hardware being more open or more closed.  You're looking at two entirely different types of stakeholder.

     

    The open metric is not flawed, it's just not valued highly by those who don't rate openness highly.  Doh! image

    Now now, don't go putting words into my mouth that I haven't said, lol.  I'm saying (quoting my previous post) "[the current definition] encourages manufactures to put more info where we can't touch it in order to get the stamp of open source approval instead of actually rewarding those who make the effort to give us more control over the equipment."

     

    This has nothing to do with me wanting openness or me wanting functionality, this is about the atmosphere we (in the broader hobbyist/hacker community sense) are encouraging.  If I'm making a board that I want hobbyist to get into then we've made it clear that it makes more sense to hide everything away in the hardware than let anyone knows it exists.  If the foundation hadn't been so open about things and hidden the files on the FAT32 partition in a non-editable memory location then all this binary blob business never would have come up.  In fact they could have claimed complete openness if they had just held off on saying until they had gotten the ARM side GPU interfaces released and hidden all the FAT32 files.

     

    And this is why I'm saying things are flawed (and not because I don't highly value openness as you've stated image) because we are by our own actions creating the framework for a loss of functionality so we can have openness.  It's like we're cutting our noses to spite or faces.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

     

    The current definitions we're working with are flawed as they encourage manufactures to put more info where we can't touch it

     

    You're confusing two things:  being more open, and having more functionality.  They're completely and utterly different concepts.

     

    Sure, those who want to use advanced but closed functions will praise their availability, but this has absolutely nothing to do with the hardware being more open or more closed.  You're looking at two entirely different types of stakeholder.

     

    The open metric is not flawed, it's just not valued highly by those who don't rate openness highly.  Doh! image

    Now now, don't go putting words into my mouth that I haven't said, lol.  I'm saying (quoting my previous post) "[the current definition] encourages manufactures to put more info where we can't touch it in order to get the stamp of open source approval instead of actually rewarding those who make the effort to give us more control over the equipment."

     

    This has nothing to do with me wanting openness or me wanting functionality, this is about the atmosphere we (in the broader hobbyist/hacker community sense) are encouraging.  If I'm making a board that I want hobbyist to get into then we've made it clear that it makes more sense to hide everything away in the hardware than let anyone knows it exists.  If the foundation hadn't been so open about things and hidden the files on the FAT32 partition in a non-editable memory location then all this binary blob business never would have come up.  In fact they could have claimed complete openness if they had just held off on saying until they had gotten the ARM side GPU interfaces released and hidden all the FAT32 files.

     

    And this is why I'm saying things are flawed (and not because I don't highly value openness as you've stated image) because we are by our own actions creating the framework for a loss of functionality so we can have openness.  It's like we're cutting our noses to spite or faces.