Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54394 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    Billy Thornton wrote:

     

    Something people seem to be misunderstand here. You don't need an open GPU...

    You do if you want to use the GPU for anything other than standard graphics.

     

    My understanding is that most GPUs are general-purpose RISC machines with some additional instructions for graphics and image processing.  They are parallel processors with supercomputer performance.  Yes, you can use them for OpenGL and other standard graphics operations, but you could also use them for non-graphical high-performance parallel processing -- if you could get at the architecture.  For example, RasPi's BCM2835 is a high-performance media engine -- plus a cheap, low performance ARM11 I/O processor.  You can use this I/O processor for anything you want, but you can only use the supercomputer for the graphics and video functions allowed by RasPi's "binary blob".  This is like buying a Cray supercomputer -- but only being allowed to use the I/O processor.

     

    This is why Parallella is such an exciting technology.  You can use the supercomputer for anything -- not just the applications the GPU supplier has decided to let you do.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    Billy Thornton wrote:

     

    Something people seem to be misunderstand here. You don't need an open GPU...

    You do if you want to use the GPU for anything other than standard graphics.

     

    My understanding is that most GPUs are general-purpose RISC machines with some additional instructions for graphics and image processing.  They are parallel processors with supercomputer performance.  Yes, you can use them for OpenGL and other standard graphics operations, but you could also use them for non-graphical high-performance parallel processing -- if you could get at the architecture.  For example, RasPi's BCM2835 is a high-performance media engine -- plus a cheap, low performance ARM11 I/O processor.  You can use this I/O processor for anything you want, but you can only use the supercomputer for the graphics and video functions allowed by RasPi's "binary blob".  This is like buying a Cray supercomputer -- but only being allowed to use the I/O processor.

     

    This is why Parallella is such an exciting technology.  You can use the supercomputer for anything -- not just the applications the GPU supplier has decided to let you do.