Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54410 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

    You're confusing two things:  being more open, and having more functionality.  They're completely and utterly different concepts.

     

    Sure, those who want to use advanced but closed functions will praise their availability, but this has absolutely nothing to do with the hardware being more open or more closed.  You're looking at two entirely different types of stakeholder.

     

    And this is why I'm saying things are flawed (and not because I don't highly value openness as you've stated image) because we are by our own actions creating the framework for a loss of functionality so we can have openness.  It's like we're cutting our noses to spite or faces.

     

    But that's exactly what I said --- that desire for openness is being confused with desire for functionality.

     

    To someone who wants openness, adding a closed feature is no benefit at all.  Only those who don't mind that the nose is closed would say that cutting it off spites their (otherwise open) face.  That analogy is emotionally biased because we don't like to lose our noses, but if you restate it with "leprous carbunkle" in place of nose, you'll see how cutting it off can be very desirable.  The leprous carbunkle is the closed feature in the analogy.

    See there you're putting words in my mouth again.  I definitily want openness, but you're stating that I can only be for openness provided I think that adding a closed feature is of no benefit.  I would argue that calling it a leprous cabunkle is equally emotionally biased because obviously that's something you'd definitely want removed.

     

    I fear, however that you're focusing too closely on a single part of my post and ignoring the greater context around it.  Namely that "[the current definition] encourages manufactures to put more info where we can't touch it in order to get the stamp of open source approval instead of actually rewarding those who make the effort to give us more control over the equipment." Now in none of my posts have I said that I want us to stop pushing for more openness, what I have said is we need to applauded the steps being done to make systems more open, rather than attacking people when they release something additional becuase they haven't released everything yet.

     

    I've also stated that this attitude is creating an atmosphere which encourages manufacture to remove functionality.  This is not, as you've mistakenly stated, because I'm confusing functionality with openness, it's because I'm taking the current attitude amongst hobbyist and looking down the road and recognizing that this will ultimately work against us.  Through pattern recognition I can look at what's going on and see that we're ultimately going to be restricting growth.

     

    Conversely if we were to focus on how open different boards were (using a weighted average rather than a blind count) and then encouraged the purchasing of boards that were more open, then the manufacturers would be motivated to open up more of the previously closed features rather than just restricting *any* use of closed systems.

     

    The current mindset actually encourages an increase of black boxes that obfuscate the system rather than encouraging manufacturers to truly open up the process.  Which is why it's so flawed.  It is actually encouraging the regression of available technology instead of furthering the amount of technology that is truly open.

     

    > And correspondingly, there is nothing wrong with pointing out that the manufacturer has delivered to the user a  programmable device which the user is being denied from programming through an artificial restriction.  Interest in open source software and open hardware is huge these days, and no manufacturer can pretend to be unaware of it.

     

    This I can fully agree with lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

    You're confusing two things:  being more open, and having more functionality.  They're completely and utterly different concepts.

     

    Sure, those who want to use advanced but closed functions will praise their availability, but this has absolutely nothing to do with the hardware being more open or more closed.  You're looking at two entirely different types of stakeholder.

     

    And this is why I'm saying things are flawed (and not because I don't highly value openness as you've stated image) because we are by our own actions creating the framework for a loss of functionality so we can have openness.  It's like we're cutting our noses to spite or faces.

     

    But that's exactly what I said --- that desire for openness is being confused with desire for functionality.

     

    To someone who wants openness, adding a closed feature is no benefit at all.  Only those who don't mind that the nose is closed would say that cutting it off spites their (otherwise open) face.  That analogy is emotionally biased because we don't like to lose our noses, but if you restate it with "leprous carbunkle" in place of nose, you'll see how cutting it off can be very desirable.  The leprous carbunkle is the closed feature in the analogy.

    See there you're putting words in my mouth again.  I definitily want openness, but you're stating that I can only be for openness provided I think that adding a closed feature is of no benefit.  I would argue that calling it a leprous cabunkle is equally emotionally biased because obviously that's something you'd definitely want removed.

     

    I fear, however that you're focusing too closely on a single part of my post and ignoring the greater context around it.  Namely that "[the current definition] encourages manufactures to put more info where we can't touch it in order to get the stamp of open source approval instead of actually rewarding those who make the effort to give us more control over the equipment." Now in none of my posts have I said that I want us to stop pushing for more openness, what I have said is we need to applauded the steps being done to make systems more open, rather than attacking people when they release something additional becuase they haven't released everything yet.

     

    I've also stated that this attitude is creating an atmosphere which encourages manufacture to remove functionality.  This is not, as you've mistakenly stated, because I'm confusing functionality with openness, it's because I'm taking the current attitude amongst hobbyist and looking down the road and recognizing that this will ultimately work against us.  Through pattern recognition I can look at what's going on and see that we're ultimately going to be restricting growth.

     

    Conversely if we were to focus on how open different boards were (using a weighted average rather than a blind count) and then encouraged the purchasing of boards that were more open, then the manufacturers would be motivated to open up more of the previously closed features rather than just restricting *any* use of closed systems.

     

    The current mindset actually encourages an increase of black boxes that obfuscate the system rather than encouraging manufacturers to truly open up the process.  Which is why it's so flawed.  It is actually encouraging the regression of available technology instead of furthering the amount of technology that is truly open.

     

    > And correspondingly, there is nothing wrong with pointing out that the manufacturer has delivered to the user a  programmable device which the user is being denied from programming through an artificial restriction.  Interest in open source software and open hardware is huge these days, and no manufacturer can pretend to be unaware of it.

     

    This I can fully agree with lol