Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54463 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    I wonder if my use of the word "confuse" is making my point get misinterpreted.  I'll try a different form of words.

     

    A desire for openness is one thing.  A desire for functionality is another thing.  Those two things are not one and the same thing.  What's more, it's perfectly possible and common that a person can want both things.  But even when a person wants both, they are still not the same thing.  They are completely different things.

     

    And that is why neither of the following two actions make sense:

     

    1. Taking a weighted average of two different things, "functionality" and "openness".
    2. Using that weighted average of two things to then modify that single thing "openness".

     

    I mean really, that would be a manifestly dreadful fudge, as well as being simply invalid.  Greater functionality can never alter the degree of openness of a product, so no, the weighted average idea makes no sense at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago

    I wonder if my use of the word "confuse" is making my point get misinterpreted.  I'll try a different form of words.

     

    A desire for openness is one thing.  A desire for functionality is another thing.  Those two things are not one and the same thing.  What's more, it's perfectly possible and common that a person can want both things.  But even when a person wants both, they are still not the same thing.  They are completely different things.

     

    And that is why neither of the following two actions make sense:

     

    1. Taking a weighted average of two different things, "functionality" and "openness".
    2. Using that weighted average of two things to then modify that single thing "openness".

     

    I mean really, that would be a manifestly dreadful fudge, as well as being simply invalid.  Greater functionality can never alter the degree of openness of a product, so no, the weighted average idea makes no sense at all.