Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54462 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    mynameisJim wrote:

     

    It would be an interesting case study to see a company open up on what had previously been tightly locked up and get hard evidence on if opening it up improved the technology.

     

    That would indeed be interesting.  I seem to recall reading some case studies on the business effects of open sourcing software by one of the many free and open source advisary bodies, but I don't recall having read anything like that regarding opening hardware.  If any reader encounters such material, please link us.

     

    On the weighted average we were discussing, I agree that it would be hard, but I do think it would be possible to take a dispassionate view and give fair rankings.

     

    There's an inherent and inescapable problem with that though.  A ranking is either going to favour one interest over another and therefore by definition not be fair to those whose main interest it ranks lower, or else it is going to rank all interests equally and hence not be a ranking at all.  Because of the variety in the target audience, there is no actual way to accomplish what you're suggesting.  The diversity precludes meaningful averaging and fair ranking, because averaging of disparate interests cannot be done and ranking itself cannot be fair.

     

    A fair report on openness and encouraging people to positively petition for more openness while using their money to support those who are making progress in the right direction will provide additional incentive.

     

    An accurate description of which parts are not currently open is completely fair.  It may not be appreciated by some people who might find it inconvenient, but it has the fairness and impartiality of hard fact.  It's hard to beat.

     

    Note however that the above doesn't preclude others from dancing tactfully around the subject and using tricks of diplomacy to help management lean more towards openness.  If you think that's going to work, by all means try it!  It's not going to change the facts about which elements are currently closed though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago

    mynameisJim wrote:

     

    It would be an interesting case study to see a company open up on what had previously been tightly locked up and get hard evidence on if opening it up improved the technology.

     

    That would indeed be interesting.  I seem to recall reading some case studies on the business effects of open sourcing software by one of the many free and open source advisary bodies, but I don't recall having read anything like that regarding opening hardware.  If any reader encounters such material, please link us.

     

    On the weighted average we were discussing, I agree that it would be hard, but I do think it would be possible to take a dispassionate view and give fair rankings.

     

    There's an inherent and inescapable problem with that though.  A ranking is either going to favour one interest over another and therefore by definition not be fair to those whose main interest it ranks lower, or else it is going to rank all interests equally and hence not be a ranking at all.  Because of the variety in the target audience, there is no actual way to accomplish what you're suggesting.  The diversity precludes meaningful averaging and fair ranking, because averaging of disparate interests cannot be done and ranking itself cannot be fair.

     

    A fair report on openness and encouraging people to positively petition for more openness while using their money to support those who are making progress in the right direction will provide additional incentive.

     

    An accurate description of which parts are not currently open is completely fair.  It may not be appreciated by some people who might find it inconvenient, but it has the fairness and impartiality of hard fact.  It's hard to beat.

     

    Note however that the above doesn't preclude others from dancing tactfully around the subject and using tricks of diplomacy to help management lean more towards openness.  If you think that's going to work, by all means try it!  It's not going to change the facts about which elements are currently closed though.