Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54464 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    jamodio wrote:

     

    Unfortunately there is and there will be no real fix for the usb issues with the Rpi. The Synopsys IP is very limited and there is not much more you can do as a workaround to make OTG to behave as a full fledged HOST implementation.

     

    The only possible fix besides the current workaround and trying to live with its limitations is to throw away the SoC and start fresh with a better USB implementation that fully supports a Host interface, but it is very unlikely that this will ever happen.

     

    While servicing USB interrupts on the VideoCore to make up for the inability of the ARM to meet the 1ms realtime response requirement when it's busy doing something else is the much-touted future solution, whether it will be done or not probably depends on whether RPF and Broadcom consider it a wise investment of time and effort (ie. money) by their skilled engineers.

     

    That in turn probably depends on whether other Broadcom SoCs also employ the same dreadful Synopsys USB controller which is the cause of all this pain in the first place.  If they do use it then that substantial development effort may be worthwhile to prevent all the affected Broadcom devices suffering the same problems as the BCM2835.  In contrast, if more modern Broadcom devices use a different and fully functional USB controller then such development might well be seen as wasted effort and not see the light of day.

     

    These two different situations could result in two different outcomes for Raspberry Pi.  Does anyone know whether the BCM11311 that has been mentioned in connection with the next-generation Pi employs the same Synopsys USB core?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago

    jamodio wrote:

     

    Unfortunately there is and there will be no real fix for the usb issues with the Rpi. The Synopsys IP is very limited and there is not much more you can do as a workaround to make OTG to behave as a full fledged HOST implementation.

     

    The only possible fix besides the current workaround and trying to live with its limitations is to throw away the SoC and start fresh with a better USB implementation that fully supports a Host interface, but it is very unlikely that this will ever happen.

     

    While servicing USB interrupts on the VideoCore to make up for the inability of the ARM to meet the 1ms realtime response requirement when it's busy doing something else is the much-touted future solution, whether it will be done or not probably depends on whether RPF and Broadcom consider it a wise investment of time and effort (ie. money) by their skilled engineers.

     

    That in turn probably depends on whether other Broadcom SoCs also employ the same dreadful Synopsys USB controller which is the cause of all this pain in the first place.  If they do use it then that substantial development effort may be worthwhile to prevent all the affected Broadcom devices suffering the same problems as the BCM2835.  In contrast, if more modern Broadcom devices use a different and fully functional USB controller then such development might well be seen as wasted effort and not see the light of day.

     

    These two different situations could result in two different outcomes for Raspberry Pi.  Does anyone know whether the BCM11311 that has been mentioned in connection with the next-generation Pi employs the same Synopsys USB core?