Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54457 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    selsinork wrote:

     

    Billy Thornton wrote:

     

    Adding stuff to chips make them more expensive just from silicon area, so be careful what you wish for. You might get better features, but you will also have to pony up more bucks.

    It's not like you'd keep the existing usb core and just add a new one. Removing a flawed piece and replacing it with a working one isn't necessarily going to take more space. That will naturally depend on the implementation details, about which we know nothing.

    As i understand it, the usb core requires a big software driver tomake it work because it doesnt do enough in hardware. Chaning to a new hardware block will almost certaily increase the size of the chip, to get that software in to hardware. but my point was actually on the ethernet point - add that and you chips get bigger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    selsinork wrote:

     

    Billy Thornton wrote:

     

    Adding stuff to chips make them more expensive just from silicon area, so be careful what you wish for. You might get better features, but you will also have to pony up more bucks.

    It's not like you'd keep the existing usb core and just add a new one. Removing a flawed piece and replacing it with a working one isn't necessarily going to take more space. That will naturally depend on the implementation details, about which we know nothing.

    As i understand it, the usb core requires a big software driver tomake it work because it doesnt do enough in hardware. Chaning to a new hardware block will almost certaily increase the size of the chip, to get that software in to hardware. but my point was actually on the ethernet point - add that and you chips get bigger.