Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54464 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    Billy Thornton wrote:

     

    I've got some pos samsung phone, some stuff on it doesnt work very well and it should.

     

    If this relates to Raspberry Pi in some way, it's not being very complimentary.  But I agree, it should work to spec, or else it's not of merchantable quality.

     

    Regarding your "0.001%", it seems that the point isn't getting across, namely that USB compliance means automatic support for everything that is class-compliant or has a driver for the architecture.  Partial percentages don't enter into this.  If Pi is USB-compliant as a USB host then it will work with 100% of USB-compliant devices subject to power, bandwidth and driver requirements being met.  No per-device development is required.

     

    I suspect that RPF/Broadcom engineers are continuing to work at the problem because that is exactly what they want to achieve --- correct USB host operation, not partial.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago

    Billy Thornton wrote:

     

    I've got some pos samsung phone, some stuff on it doesnt work very well and it should.

     

    If this relates to Raspberry Pi in some way, it's not being very complimentary.  But I agree, it should work to spec, or else it's not of merchantable quality.

     

    Regarding your "0.001%", it seems that the point isn't getting across, namely that USB compliance means automatic support for everything that is class-compliant or has a driver for the architecture.  Partial percentages don't enter into this.  If Pi is USB-compliant as a USB host then it will work with 100% of USB-compliant devices subject to power, bandwidth and driver requirements being met.  No per-device development is required.

     

    I suspect that RPF/Broadcom engineers are continuing to work at the problem because that is exactly what they want to achieve --- correct USB host operation, not partial.