Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54507 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

     

    Actually that's very much my point, non-compliant devices are routinely given the stamp of approval.  And non-compliant devices are really advertised as such.  The end result is that people plug a USB device into the pi expecting it to work like it should having no knowledge that it's not following the standard and then discussions about them arrise.

     

    But that uncompromising position on non-compliant devices (may they burn in ignomy) is matched with an equally uncompromising position on hosts that don't work correctly with fully USB-compliant devices, especially class-compliant devices in the most common classes.  Engineering is an iterative and evolving process and some things take time to get right, and that's OK, I can wait, and the devs are heading in the right direction.  But it has to be fixed.

    lol, you act like I'm disagreeing with you, but right after the part of my post you quoted, I go on to state that I agree with this and that the Pi has something to be fixed (and from what I can tell from the USB threads is actively being worked on).

     

    > Stuart Wrote: Yes, pretty much.  But it's not just jamesh saying it, it's everyone associated with the Raspberry Pi Foundation who posts on their forums except for dom and gsh.  It's cognitive dissonance, they want to believe the Raspberry Pi is flawless and can't deal with it when any evidence to the contrary is presented.  This is the cause of the denial and minimisation.

     

    >But denial and minimisation is an improvement over the total silence which was the RPFs initial non-response to the USB problems when they were first pointed out and the subsequent 'it's caused by an inadequate power supply" catch-all explanation.

     

    I agree that there was a lot of knee jerk reaction referring people to the power supply.  Of course, reading over the old usb threads there was also a lot of problems caused by those early days of the limiting fuse on the USB ports and improper power supplies were quite the problem and not everyone who suggested it as a starting point of troubleshooting was trying to say that was the only possible issue, just that it was the starting point.  There were also plenty of people who attacked anyone for asking how their PSU looked just to kick things off.  Extremism works on all sides of an issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Morgaine Dinova wrote:

     

    mynameisJim wrote:

     

    Actually that's very much my point, non-compliant devices are routinely given the stamp of approval.  And non-compliant devices are really advertised as such.  The end result is that people plug a USB device into the pi expecting it to work like it should having no knowledge that it's not following the standard and then discussions about them arrise.

     

    But that uncompromising position on non-compliant devices (may they burn in ignomy) is matched with an equally uncompromising position on hosts that don't work correctly with fully USB-compliant devices, especially class-compliant devices in the most common classes.  Engineering is an iterative and evolving process and some things take time to get right, and that's OK, I can wait, and the devs are heading in the right direction.  But it has to be fixed.

    lol, you act like I'm disagreeing with you, but right after the part of my post you quoted, I go on to state that I agree with this and that the Pi has something to be fixed (and from what I can tell from the USB threads is actively being worked on).

     

    > Stuart Wrote: Yes, pretty much.  But it's not just jamesh saying it, it's everyone associated with the Raspberry Pi Foundation who posts on their forums except for dom and gsh.  It's cognitive dissonance, they want to believe the Raspberry Pi is flawless and can't deal with it when any evidence to the contrary is presented.  This is the cause of the denial and minimisation.

     

    >But denial and minimisation is an improvement over the total silence which was the RPFs initial non-response to the USB problems when they were first pointed out and the subsequent 'it's caused by an inadequate power supply" catch-all explanation.

     

    I agree that there was a lot of knee jerk reaction referring people to the power supply.  Of course, reading over the old usb threads there was also a lot of problems caused by those early days of the limiting fuse on the USB ports and improper power supplies were quite the problem and not everyone who suggested it as a starting point of troubleshooting was trying to say that was the only possible issue, just that it was the starting point.  There were also plenty of people who attacked anyone for asking how their PSU looked just to kick things off.  Extremism works on all sides of an issue.