Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54764 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 13 years ago

    Spring greetings to you all ...  this thread has brought me out of my forum sabatical, naughty naughty. image

     

    Seeing the Slashdot thread on BeagleBone Black made me warp over to here post haste, as I guessed you would all be talking about it ... and you were, hehe.  I agree with everything that's been said.

     

    Two additional bits of information that slightly change the picture:

     

    • Farnell UK says "18584 will be available for delivery on 3 May, 2013", so they're clearly taking this seriously and expect BB Black to sell in much higher volumes than the first BeagleBone.  No surprise of course, price is king.

     

    • The BeagleBone's TI Sitara AM3359 contains a pair of integer-only realtime processors running at 200MHz, the Programmable Realtime Unit Subsystem or "PRU".  These can provide waaaaaaay better hard realtime interfacing performance than any program running in Linux user-space, so for hardcore techies who aren't afraid of getting their hands dirty with some pretty simple assembler, the BeagleBone is lightyears ahead of the Pi in interfacing capability.

     

    Success has very little to do with engineering merit though, so I won't be making any guesses about how popular this new board will become.  However, for myself, the Pi Model B is now totally dead in the water since it lost its only advantage, which was price.

     

    Needless to say, BeagleBone Black is on my shopping list as soon as they're in stock. image

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to morgaine

    These can provide waaaaaaay better hard realtime interfacing performance than any program running in Linux user-space,

     

    There are also several real-time Linux kernel patch sets (Xenomia is one) that can provide way better real time (hard and soft) performance running in "RT" user space than anything running

    in "normal" user space. They also supply full RT APIs to work with and hardware (when available) supported floating point if you need it. Any RT kernels avaialable for the PRUs ?

     

      If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player

     

    I bought one off of Ebay several months ago which is one of the reasons I'm not as interested in the Cubieboard as I use to be. It does have wi-fi and Ethernet and although it is bit short on the

    user I/O it does also have serial, I2C (have to add a header), IR remote control and a SATA 2 interface. There are several web sites that provide Linux for the A10 and it already comes with what

    I think is an Android OS for the media player operation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to morgaine

    These can provide waaaaaaay better hard realtime interfacing performance than any program running in Linux user-space,

     

    There are also several real-time Linux kernel patch sets (Xenomia is one) that can provide way better real time (hard and soft) performance running in "RT" user space than anything running

    in "normal" user space. They also supply full RT APIs to work with and hardware (when available) supported floating point if you need it. Any RT kernels avaialable for the PRUs ?

     

      If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player

     

    I bought one off of Ebay several months ago which is one of the reasons I'm not as interested in the Cubieboard as I use to be. It does have wi-fi and Ethernet and although it is bit short on the

    user I/O it does also have serial, I2C (have to add a header), IR remote control and a SATA 2 interface. There are several web sites that provide Linux for the A10 and it already comes with what

    I think is an Android OS for the media player operation.