Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54760 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    To me its a like comparing BetaMax to VHS.  The Raspberry Pi is cheaper but has less features where as the BeagleBone has more of the features I really want for $10 more (flash memory, more IO, a better and established shield/cape system, more processing power).  If I have a new project I will be looking at BeagleBone. 

     

    Unless TI starts marketing the bat snot out of the unit it will never come close to the volume of the Pi.  Remember that Pi had nearly two years of press before it came out. Most of the press was about the little guy making his dream come try.  The BB Black hardly had any press.  The only way I can see TI getting the word out is as a comeback story that harkens back to old 8 bit PC days.  Otherwise it stay a hobby/engineering tool.

     

    Will I use a Raspberry Pi?  Model A boards yes.  I like the processing power but with a low power consumption for the cost of an Arduino. Model B board now that BB Black is out?  Very unlikely.  I get access to Android and Ubuntu with BB Black. That means I can use PhoneGap/Cordova and Mono to build my apps faster than I can in Python.  Also it has some extra features like true serial connection, power and reset switches, and mounting holes.

     

    I'm not trying to start a flame war.  I like playing with my Pi but this maybe a better option for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Ervin Kosch wrote:

    I get access to Android and Ubuntu with BB Black. That means I can use PhoneGap/Cordova and Mono to build my apps faster than I can in Python.

    Actually I think that having the A8, not having to do a Raspbian style hf rebuild, and therefore being able to use un-altered distros is a very strong point in the BBB's favour. Thanks for mentioning it.

    I'm not trying to start a flame war.  I like playing with my Pi but this maybe a better option for me.

    Oh, I like mine too. And I agree with a lot of your other points.  The BBB is the closest to the Pi in price that I've seen while being better in some ways, so I think there will be lots of comparisons being made that don't really work when you try to compare the Pi to something like the Sabre-Lite at 6x the price.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

    No, I'm not. I think the worst case scenario you just described is not realistic for several reasons. Raspian is the official RPF distribution. There are now over 500,000 Raspberry Pi's out there, most using Raspian. There

    is nothing to stop another group of people from taking over or forking Raspian if the current maintainers stopped, and I don't see the RPF not trying to find, or having a lot of trouble finding other people to maintain it if that

    happened.

     

    We'll agree to disagree then. 

     

    That said, it's interesting to look back at the RPF history. Ubuntu was originally going to be the official RPF distribution, until Ubuntu dropped support. Nobody stepped up to take on a port. Next Fedora was to be the official RPF distribution, but Fedora weren't interested, Seneca stepped in (possibly with some help from the RPF) and produced a port, problems with that port caused it to be fairly quietly dropped by the RPF. Every now and again we hear there may be another version, but again nobody seems to have stepped up to help them with it.

     

    Mike Thompson and Peter Green deserve a lot of credit for what they've done with Raspbian, long may it continue. But so far, Mike and Peter appear to be the only ones to have sucessfully taken on such a project. As far as I'm aware it's still mostly a two man show and if I believe what's out there to be read it may even be that Peter has taken on the lions share.

    So with other past failures, partial or otherwise, I don't believe the argument is as easily dismissed as you make out, if it were then surely they'd have found someone to do the same for Ubuntu or Fedora ?

     

    And Liz has said, back on the 1st of March that there's at least a million sold: http://www.raspberrypi.org/archives/3375 so there's a potentially much bigger pool of talent available than you suggest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Mike Thompson and Peter Green deserve a lot of credit for what they've done with Raspbian, long may it continue. But so far, Mike and Peter appear to be the only ones to have sucessfully taken on such a project. As far as I'm aware it's still mostly a two man show and if I believe what's out there to be read it may even be that Peter has taken on the lions share.

     

    Fortunately that problem will disappear as soon as RPF brings out a next gen Raspberry Pi based on a SoC with a more modern ARM, which can then be supported by standard portable Linux distributions.  That will undoubtedly happen, if we make the very reasonable assumption that the RPF project continues and prospers.  The only question is when.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    > The only question is when.

     

    We have some clues.

    The 1st gen RPi was based on the same cpu as the Roku 2,

    and both were announced mid 2011.

    The Roku 3 became available recently, using the next generation

    Broadcom cpu with dual core Cortex A9, with only a slight increase

    in price over the Roku 2.

    Sony has already mentioned the 2nd gen RPi.

    Liz has downplayed the Sony announcement.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    The only question is when.

    I've not been following it closely, but everytime I see some mention of some form of updated Pi the official answer seems to come back as 'not for the forseeable future'. Possibly that's understandable - they still need to make some money from the long awaited camera module, try getting them into schools, and then there's that other as yet unused connector they might want to use.

    So while you're right, would you bet on the 'when' being anytime soon ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Sony has already mentioned the 2nd gen RPi.

    Pointer ?

    Liz has downplayed the Sony announcement.

    One of the places I worked had a running in-house joke that the lifetime of a particular product was only about six weeks. There'd then be a 'new' product, with different code names etc. usually the only difference was a minor tweak here and there, or no difference at all apart from some plug in part.

     

    So I can understand some downplaying as a 2nd gen RPi could mean almost anything while quite rightly being seen as a 'new' product by Sony.  We'll find out sooner or later, but neither a minor revision or a fully new design would surprise me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    second generation Pi

    http://www.element14.com/community/message/73959

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Without knowing why each of them decided to turn RPF down knowing the history doesn't say much of anything useful. I'm not sure if any of the ones you mentioned

    already had ARM ports or not, I know Debian did. It could have been that they were already too busy or didn't think that there would be enough interest in the PI to

    make it worth their time and effort. But strangely enough, now there is a Fedora port, and an Arch port, and a BSD port. Did I miss any ?

     

    One last point. Being officially supported by Debian does not mean that if the distribution maintainers decide to call it quits Debian will step in and help. This leaves

    any distribution officially supported or not in the same boat as Raspian should they quit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So while you're right, would you bet on the 'when' being anytime soon ?

     

    I have no idea, but I do think that it's likely that their next-gen Pi plans have just accelerated with the release of BeagleBone Black.  Now they finally have competition within their price niche, whereas before they didn't.

     

    This assumes of course that they are sensitive to competition, but I think that they are, judging by the way that they're downplaying the significance of BBB in typical fanboi style.  I don't want to guess at dates or even years, but they don't have forever to respond or they'll lose their market completely.  Time marches on, and clearly the competition has arrived.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    Did I miss any ?

    http://en.wikipedia.org/wiki/Raspberry_pi says yes, you missed quite a few, but probably a lot of them are much less mainstream. Curiously, Fedora is missing from that list.

    http://elinux.org/RPi_Distributions has an even more impressive list, a bunch of which I've never even heard of.

     

    Package counts are interesting, I was way off with 10000 packages in Debian it seems as they quote 35000+.

     

    The one mainstream choice I'd previously thought was conspicuously absent, OpenSUSE seems to be there as well.

     

    However reading the post on the RPF forums linked to from the OpenSUSE entry suggests there may be other troubles ahead for Arm - not just the Pi - with the NWFPE removal from upstream kernels due to licensing.

    Should be interesting as it could have all sorts of effects if you can no longer distribute the old code while not having a way forward. Sounds like this will break all the softfloat distros, likely some of the hardfloat ones depending on the exact VFP, and upstream might only want to deal with newer CPU's - leaving the RPF to re-engineer a solution for the particular combination we have.

     

    So, something learned for me there..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    You missed the sarcasm (OK it might not have been obvious) and the point (the Pi has become important enough for several of the ones that passed up on the opportunity earlier to

    port to it now).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    You missed the sarcasm (OK it might not have been obvious) and the point (the Pi has become important enough for several of the ones that passed up on the opportunity earlier to

    port to it now).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    You missed the sarcasm

    Not so much. But we still fundamentally disagree on that point. I still don't think that an unofficial, one man port is anything like the same as a fully upstream supported port done by the distro themselves.

    I do however value the interesting discussion and the differeing viewpoint, even when I suspect we'll never agree on that particular subject image