Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54138 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    gdstew over 13 years ago

    I'd like to add another pro for the BeagleBoard Black.

     

    With the exceptions of the integer real time processors PRU-ICSS (not sure at this point why that is), and the PowerVR GPU for

    well known reasons, the AM3359 technical documentation from TI is excellent to the point of overwhelming. The Technical Reference

    Manual is over 4000 pages. No I did not accidentally add any zeros !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    The Technical Reference Manual is over 4000 pages. No I did not accidentally add any zeros !

    One of the other boards I have some interest in is the Sabre-Lite, Freescale have a ref manual for their iMX6 that's bigger, close to 6k pages if memory serves.

    Similar omissions for the GPU and their secure boot module though.

     

    I couldn't agree more, copious documentation like these two have is the way forward and really should become the norm instead of the exception.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    The Technical Reference Manual is over 4000 pages. No I did not accidentally add any zeros !

    One of the other boards I have some interest in is the Sabre-Lite, Freescale have a ref manual for their iMX6 that's bigger, close to 6k pages if memory serves.

    Similar omissions for the GPU and their secure boot module though.

     

    I couldn't agree more, copious documentation like these two have is the way forward and really should become the norm instead of the exception.