Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 717 subscribers
  • Views 54082 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Using the PRU will limit your design to just one family of SOC's.

    If tomorrow a new SOC comes out with twice the speed for half the price of the TI chip, you won't be able to use it.

    Fine tuning Linux boot behavor to decrease startup times is again a very time consuming and fustrating job.

    Yes, 10000+ is a totally arbitrary number, but if the knowledge how to use a real time linux or posix kernel isn't available, it's hard to predict how long it will take to create a design with that technology, and I rather play on safe and avoid the risk.

    We probably both are right in our descisions based upon the products we create.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    Fine tuning Linux boot behavor to decrease startup times is again a very time consuming and fustrating job.

    It's not really so bad. You just need to start with the assumption that for something embedded you really don't want a full blown desktop distro on there. Once you're happy with making that decision you can get rid of a load of crap in the startup that's simply not necessary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    Fine tuning Linux boot behavor to decrease startup times is again a very time consuming and fustrating job.

    It's not really so bad. You just need to start with the assumption that for something embedded you really don't want a full blown desktop distro on there. Once you're happy with making that decision you can get rid of a load of crap in the startup that's simply not necessary.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Regarding startup times, it's interesting to ponder that an AM3359 could in principle be made to initialize and preload its PRUs on startup even before commencing the Linux boot process.  This would give such an embedded system a near instant-start for many interfacing applications, delaying only the higher level processing until Linux has come up fully.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to morgaine

    Industrial minimodule using these AM335x PRUs described in "TQMa335: The CortexTm A8 module with PRU support", and more detail of same.