Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Pi vs BeagleBone-Black
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 358 replies
  • Subscribers 714 subscribers
  • Views 55822 views
  • Users 0 members are here
  • raspberry_pi
  • bb_black
Related

Pi vs BeagleBone-Black

e14 Contributor
e14 Contributor over 13 years ago

So, just over a year on from the initial availability of the R-Pi and the new BeagleBone Black is upon us.  They've obviously taken a leaf out of the RPF's playbook and produced a cost reduced version at a price only marginally above the Pi.

 

I find it interesting that the compromises are very different, for example there's a proper PMIC and the ethernet is not troubled by being connected to USB, however the on-board HDMI seems less capable.

 

Other differences are in the documentation, I'm currently viewing the pcb gerbers for the beaglebone..  Have yet to see any sign of those for the R-Pi a year later. There's even an up to date devicetree capable kernel too.

 

Technology has also moved on somewhat, we get a 1GHz Cortex A8 which is better than the Pi, along with various other stuff and lots more GPIO's too.

 

Ok, so it's clear that I like the look of the new beaglebone, and given the price I'm likely to put any further R-Pi plans on hold until I have a chance to play with this. It's also making things like the Olinuxino-maxi I bought recently look very slow/expensive while still being cheaper than the similarly specced Olinuxino-A13

 

Some details of the beaglebone-black here http://circuitco.com/support/index.php?title=BeagleBoneBlack

 

What do the rest of you think ?   I don't expect this to displace the Pi anytime soon, but I expect it to be very attractive to those people who don't simply want to put XBMC on it and duct tape it to the back of the TV..

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines. It will cost more than a Pi, but it comes with a supply and a housing. It also has a vga output and connector fitted. It has wifi and ethernet embedded if I remember well. There even is the Mele A2000G with 1Gig of ram.

    For GPIO, I prefer to use a dedicated microcontroller connected to the linux board with an usb interface. This approach might be a bit more expensive, but it makes it possible to switch from one linux board to another without much hassle. It also makes the system responsive to io changes after a fraction of a second instead of several seconds needed to boot the system. Maybe it's just me being conservative and used to embedded design on 8 bit microcontrollers. Linux adds connectivity to it and makes easy in system programming possible.

    The Mele also uses the allwinner A10 soc, so booting linux is possible from the sd card. Placing it on the internal flash memory of the player should be possible as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Luc Cool wrote:

     

    If finding a cubieboard is a problem, you could take a look on Ebay at the Mele A1000 media player. It's pretty much a cubieboard without the gpio lines.

    At least for me, it's the GPIO that makes or breaks the device, without them I'm much less interested.

     

    It will cost more than a Pi,

    Approx 60 GBP, so around twice what the Pi costs. Sure it's not a straight comparison.

     

    The A10 looks like it should be a good SoC and so far the cubieboard looks to be the closest to the sort of board I'm interested in. The danger, as always, is that something better and cheaper may come along by the time they start appearing in volume.

     

    Either way, interesting times, and I'm really hoping we'll see more and more devices of this type.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    What the raspberry pi foundation lying ?

    Who would have thunk it ?

     

    Actualy its ridiculous, they want everyone to think its an open hardware project despite the fact that you cannot buy the processsor unless you sell your soul to Broadcomm.

    and wow they are going to release the gerbers, big deal, Ive got the schematic I could do my own layout if I wanted, only trouble is......its not open hardware and you cannot buy the processor.

     

    Seriously stay away from the raspberry pi, it started life as an educational toy, got hijacked by some very strange people who think every embedded system has to run linux and several of my clients have tried to use it as the basis of their projects only to regret it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The article in wired was pretty tyipcal of how they work, don't talk to engineers who have any experience of designing embedded systems, talk to jouralists who have not the slightest idea and they will repeat any bullshit you tell them if you take them to lunch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The article in wired was pretty tyipcal of how they work, don't talk to engineers who have any experience of designing embedded systems, talk to jouralists who have not the slightest idea and they will repeat any bullshit you tell them if you take them to lunch.