Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi HDMI Cutting Out
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 707 subscribers
  • Views 2317 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi HDMI Cutting Out

e14 Contributor
e14 Contributor over 13 years ago

Hi All,

 

 

My Raspberry Pi HDMI keeps cutting in and out, it seems especially when the CPU is running high.  I have tried 3 different power supplies (ranging 1AMP to 2.1AMP), and they all seem to exhibit the same issue.  Any help would be appreciated, thank you.

 

Regards

Ray

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 13 years ago

    My guess is that while your power supply is fine, your Micro USB cable may have very thin conductors which can cause a substantial voltage drop when RasPi's CPU needs extra current.  Another possibility is excessive drop over polyfuse F3 when the current is high.

     

    There are other possibilities as well.  Take a look at the RasPi Troubleshooting wiki: http://elinux.org/R-Pi_Troubleshooting#No_HDMI_output_at_all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago

    My guess is that while your power supply is fine, your Micro USB cable may have very thin conductors which can cause a substantial voltage drop when RasPi's CPU needs extra current.  Another possibility is excessive drop over polyfuse F3 when the current is high.

     

    There are other possibilities as well.  Take a look at the RasPi Troubleshooting wiki: http://elinux.org/R-Pi_Troubleshooting#No_HDMI_output_at_all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    Thanks John.  I will check out that link.  What would cause the current to be high?  If the devices attached are using too much power?  Is there a limitation to what can be attached to the Pi?  I'll see if I can dig up another micro-usb cable to try too.

     

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    Ray Price wrote:

     

    Thanks John.  I will check out that link.  What would cause the current to be high?  If the devices attached are using too much power?  Is there a limitation to what can be attached to the Pi?  I'll see if I can dig up another micro-usb cable to try too.

     

    Thank you!

    Here's what the RasPi Hardware Wiki has to say about power: http://elinux.org/Rpi_Hardware#Power

     

    Basically, RasPi model B uses up to 700 mA though it's unclear whether that includes 100 mA each for two low-powered USB devices and any budget for the GPIO.  Your 1A supply should be fine.

     

    However, if your Micro USB cable or polyfuse F3 is iffy, the normal 700 mA could cause enough of a voltage drop across one or both components to drop RasPi's 5V below its minimum 4.75V.  Measuring the voltage between TP1 and TP2 as shown in both the wikis I linked to will tell you if your 5V is below spec.  Even if the 5V is low, you might be able to fix your HDMI problem with "config_hdmi_boost=4" as suggested in the Troubleshooting Wiki linked above.

     

    When I was first trying out my RasPi I had an iffy power supply and cable.  My DVI-D monitor worked fine at 4.65V and above, but below that it would first show random dot patterns and then blank out completely.  Sometimes it would be fine unless I compiled, and then the extra CPU activity dropped the voltage enough to show random dots, which would vanish when the compile completed.  Kind of a cute "feature", actually.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to johnbeetem

    When I first got my Pi, the 1A supply worked at first, then wouldn't.

    A few versions later, I finally got one that would work reliably.

     

    Even the USB outlet type models had issues, and that included the 2A version I got with the Toshiba Tablet.

     

    I seriously believe most of these aren't designed as Power supplies, but chargers for the battery which is most likely a 3.6v LiOn or similar.

     

    I did check most of the cables, and while they have a very small voltage drop, the biggest drop was the Polyfuse.

     

    The HDMI boost didn't seem to help me, but it might be worth a try.

     

     

    Interestingly, my son could run his from the USB outlet on his Netbook.!

     

     

    Mark