Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New to Raspberry PI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 709 subscribers
  • Views 2696 views
  • Users 0 members are here
  • image
  • raspberry_pi
  • sd_card
  • installation
Related

New to Raspberry PI

e14 Contributor
e14 Contributor over 13 years ago

Hello I can not seem to get started with my PI. I have run dd on my Peppermint Linux OS to the SD card, which completed sucessfully. How ever the installl image will not boot on the PI.

 

I have no idea what to do next. Please help.

 

Regards.

  • Sign in to reply
  • Cancel
Parents
  • pjc123
    pjc123 over 13 years ago

    Look here, under "Create your own":

     

     

    http://elinux.org/RPi_Easy_SD_Card_Setup

     

     

    Use the Raspbian "Wheezy" image.  If you have a Windows computer, Win32DiskImager is the easiest method to write to the sd card, but there are instructions here on using "dd" as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • pjc123
    pjc123 over 13 years ago

    Look here, under "Create your own":

     

     

    http://elinux.org/RPi_Easy_SD_Card_Setup

     

     

    Use the Raspbian "Wheezy" image.  If you have a Windows computer, Win32DiskImager is the easiest method to write to the sd card, but there are instructions here on using "dd" as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to pjc123

    Thanx to both of you. I think pjc123's reply is closest to what I need. I did not mean casuse anyone to think that I am attempting to boot Raspbian on my X86. In fact I did say that is what I did not do and therefore I have no real way to test the image as it was failing on my PI. Either one or both of those links will help me write the image as long as they are not Windows dependent. I am not at my work PC now so I will have to thank you and get at this task tomarrow.

     

    Regards.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pjc123
    pjc123 over 13 years ago in reply to e14 Contributor

    As a side note, since so many people make the same mistake, when you do the checksum (SHA-1) check on the downloaded image file, you perform it on the .zip file not the unzipped file.

     

     

    Also, here is the main page of that wiki, which has a ton of information regarding the raspberry pi:

     

    http://elinux.org/RaspberryPiBoard

     

     

    and here is a good series of magazines for beginners.  Press the arrow directly under the displayed magazines to get to all the older issues:

     

    http://www.themagpi.com/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to pjc123

    Actually I did not think to check the hash. Very bad. Also oddly enough I seem to resort to win32 md5 utilities for what ever reason. I think it is do to the fact that there are so many related and confusing md5 options, most of which that do not do what I need. That said I think there is reason to trust this md5 hash checker.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pjc123
    pjc123 over 13 years ago in reply to e14 Contributor

    I have gone through various checksum programs on Windows over the years, but the latest one I found is the best and quickest to use, called HashTab. When you right click on a file in Windows Explorer and select Properties, you can see that HashTab adds a new tab called “File Hashes”, and it can generate pretty much every checksum out there.  I can't remember offhand what Linux program that I use.

     

    http://www.implbits.com/HashTab.aspx

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to pjc123

    Yeah the win32 did fail but I simply used the help pages that were linked here and the command line md5 option worked for me.

     

    How ever I am still not getting my PI to boot. I am begining to wonder if my PI has hardware issues. But I am going to plod on and try the net install option. I forget what it is called. But it seems like the best I can do at this point.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pjc123
    pjc123 over 13 years ago in reply to e14 Contributor

    Note that there is a very small 0.02% return rate of all raspberry pis, and out of that, half of those are testing OK and never had a problem in the first place; so don't rush to return it right away (The number one issue appearing to be inadequate power supplies and/or power usb cables).  When you say that it will not boot, what are you basing this on?  Are the LED's indicating that it is not booting, (Which is what you should go by), or the fact that there is no display on the monitor?  First, go through the following troubleshooting steps, as they resolve most problems:

     

     

    http://elinux.org/R-Pi_Troubleshooting

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to pjc123

    > Note that there is a very small 0.02% return rate of all raspberry pis, and out of that, half of those are testing OK and never had a problem in the first place;

     

    I am a bit doubtful of your figures.  If around 1.2M RPi's are sold per year, or about 100K per month,

    and .02% are returned, that would be 20 units returned per month.  If half of those tested OK,

    that would be 10 OK units returned per month.    However, the Hynix memory incompatibility

    alone reportedly accounts for as many as 5 OK units in a single day, which is not surprising

    because the Debian Wheezy soft-float version on the official download page apparently still

    has the obsolete firmware, as does the latest Fedora download, as well as many pre-loaded

    SD cards still being sold.  And there are lots of reasons besides the Hynix issue for people to

    mistakenly believe their RPi is faulty.

     

    Since Farnell manufactures all their RPi's in the well-regarded Sony plant, I would expect their

    return rate to be even less than the overall rate, giving E-14 something to really brag about.  

    But nothing but silence.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pjc123
    pjc123 over 13 years ago in reply to e14 Contributor

    The quote from the raspberry pi organization yesterday was "At the moment, we see returns in the order of about 0.02% of all units".  So yes, sure, they could have waited until returns were at a minimum to make that comment.  You would have to argue with them, not me.  In any event, supplying a device with no certified or included peripherals, having people order parts anywhere at any price or of any quality, and add to that many users with little or no knowledge of electronics, computers, programming, or troubleshooting skills, well I am not at all surprised that they are getting a very high return rate of working pis.  If it wasn't for these forums, it would be much, much higher.  Maybe their intent is to teach troubleshooting skills!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to pjc123

    > The quote from the raspberry pi organization yesterday was "At the moment, we see returns in the order of about 0.02% of all units".

     

    I have no idea how to parse that sentence.  As you note, "At the moment" could mean just about anything.

    As could "we see".  Is the RPF claiming to see all the returns?

    Could it mean that today's mail bag brought in about 0.02% of all units shipped this month?

     

    They have always claimed that OK units were about half of all returns, but I see no logical reason

    why the number of OK units should decline at exactly the same rate as the number of broken units.

     

    If they are doing something to reduce the number of faulty units, like attaching the big capacitor better,

    or using a more sturdy SD card socket, that would be nice to know, but we don't hear anything along those lines.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    However, the Hynix memory incompatibility

    alone reportedly accounts for as many as 5 OK units in a single day, which is not surprising

    because the Debian Wheezy soft-float version on the official download page

     

    The official distribution is the Raspian hard float version so unless you have some numbers to show that the

    Debian distribution is a significant part of the problem I don't see how that is relevant.

     

    as does the latest Fedora download,

     

    Ditto.

     

    And there are lots of reasons besides the Hynix issue for people to

    mistakenly believe their RPi is faulty.

     

    Real strong point you're making there.

     

    Since Farnell manufactures all their RPi's in the well-regarded Sony plant, I would expect their

    return rate to be even less than the overall rate, giving E-14 something to really brag about.  

    But nothing but silence.

     

    Which proves absolutely nothing at all unless there is some rule I am not aware of that requires

    companies to brag about how well they do their jobs.

     

    I have no idea how to parse that sentence.  As you note, "At the moment" could mean just about anything.

    As could "we see".  Is the RPF claiming to see all the returns?

    Could it mean that today's mail bag brought in about 0.02% of all units shipped this month?

     

    How about these things vary month to month statistically speaking and this is what we are seeing now.

    Unless of course there is some deeply hidden and sinister ulterior motive that lurks behind the statement.

     

    If they are doing something to reduce the number of faulty units, like attaching the big capacitor better,

    or using a more sturdy SD card socket, that would be nice to know, but we don't hear anything along those lines.

     

    Again this proves nothing. They are not required to tell you or anybody else what their QC is (or is not) doing.

    It would be nice if they did, but I have not seen either of the two problems you specifically mentioned on any

    of the three I own. I especially like the big capcitor one as I have not heard anything about this for many months

    now. Maybe they fixed it and just considered it something they should do without bragging about it. Then again,

    maybe not .....