Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Sainsmart 3.2 TFT + PI = Frustration
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 707 subscribers
  • Views 2369 views
  • Users 0 members are here
  • helpme
  • pi
  • raspberrypi
Related

Sainsmart 3.2 TFT + PI = Frustration

e14 Contributor
e14 Contributor over 13 years ago

I an a NOOB. No two ways about it. But I do know that I dont want to depend on shields to get things added. That being said:
I have a 3.2" Sainsmart touch sensitive TFT display and I want to use it with my PI. this is proving to be next to impossible as all the guides out there dont do a very good job for someone at my skill level.
I am hoping to lean on this amazing community to help me with some answers. I need to know how to pin the display to my PI and what drivers I will need to push it. I am asking this as we are mentoring some kids this summer in all things STEM and I thought it would be a cool takeaway for all of them to build a miniature MAME (roms) gaming box. Just a little something to bridge the gap! IF ANYONE could help I and the kids would be greatly appreciative. Just keep in mind any response will have to be VERBOSE as I am a noob image. I have attached all the files i have on the display.

Thanks in advance!    

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    From looking at the SainSmart LCD link, it seems it has the SSD1289 LCD controller.

     

    You may have seen this already, there's a long thread on the RasPi forum about getting LCD with this controller to work:

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=64&t=33679

     

    And a video:

    https://www.youtube.com/watch?v=ES-Fg1-PuEw

     

    I think the approach used there is to use some shift registers to use SPI to talk to the LCD in order to save GPIO pins.

    That may or may not be fast enough for what you want to do, but it might get you a quick start if you want to get something to work quickly.

    The video shows the response time being "ok" for the linux boot sequence, hard to tell if the lag is from the Pi itself or the SPI->parallel conversion.

     

    HTH,

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • guzunty
    guzunty over 13 years ago in reply to e14 Contributor

    Michael P wrote:

     

    I think the approach used there is to use some shift registers to use SPI to talk to the LCD in order to save GPIO pins.

     

    Exactly. That was the exact purpose of adding the programmable logic. Its cheaper and smaller than discrete logic these days, not to mention adding buckets of flexibility.

     

    Wow, they even have X working, I'm officially impressed. Mame should not be a problem then.

     

    Thank you Michael, for a very helpful couple of links.

     

    best,

     

    Derek.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • guzunty
    guzunty over 13 years ago in reply to e14 Contributor

    Michael P wrote:

     

    I think the approach used there is to use some shift registers to use SPI to talk to the LCD in order to save GPIO pins.

     

    Exactly. That was the exact purpose of adding the programmable logic. Its cheaper and smaller than discrete logic these days, not to mention adding buckets of flexibility.

     

    Wow, they even have X working, I'm officially impressed. Mame should not be a problem then.

     

    Thank you Michael, for a very helpful couple of links.

     

    best,

     

    Derek.