Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Camera Module - cable length....
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 706 subscribers
  • Views 3320 views
  • Users 0 members are here
  • raspberry_pi
Related

Camera Module - cable length....

e14 Contributor
e14 Contributor over 13 years ago

Hi!

 

I just found the CAMERA Module for the Raspberry Pi and have a question for that.

 

Is it possible to extend the camera "cable"? What could be the maximum length then?

 

I am thinking about a special application where I need to push the camera with a special rod and the distance should be apr. 60m...... The camera is build into the a "Head" at the front end of the pushrod cable and the rapberry pi acts as recording device at the other end.....

 

Any ideas?

 

Thanks

 

TV

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 13 years ago

    Hi Thomas,

    I don't believe that this will work, if the camera board has just a parallel interface with 3.3v logic. The drivers on the camera won't have have enough drive to rapidly send 1s and zeros on a long cable, because of the capacitance, it will alter the shape of the waveform. Maybe the camera board sends using some other technology, but you'd need to check with the RPI foundation.

    Some people may suggest screened cable but that won't help you. Some (not all) possible solutions are to:

    1. Remotely mount the RPI too, and use Ethernet which will be fine for 100m

    2. Use an analog camera and coax, and no RPI - this uses a transmission technology known as "transmission line" (same as Ethernet) which in theory can be as long as you like - in practice there will be loss

    3. Use an analog camera and wireless technology and no RPI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago

    Hi Thomas,

    I don't believe that this will work, if the camera board has just a parallel interface with 3.3v logic. The drivers on the camera won't have have enough drive to rapidly send 1s and zeros on a long cable, because of the capacitance, it will alter the shape of the waveform. Maybe the camera board sends using some other technology, but you'd need to check with the RPI foundation.

    Some people may suggest screened cable but that won't help you. Some (not all) possible solutions are to:

    1. Remotely mount the RPI too, and use Ethernet which will be fine for 100m

    2. Use an analog camera and coax, and no RPI - this uses a transmission technology known as "transmission line" (same as Ethernet) which in theory can be as long as you like - in practice there will be loss

    3. Use an analog camera and wireless technology and no RPI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    Hi Thomas,

    I don't believe that this will work,

    You'd be wrong...

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=43&t=43737&sid=419088a3e7ea47166e240dfef5fa8bd1&start=22

     

    http://www.bitwizard.nl/catalog/product_info.php?products_id=146

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    That is interesting, maybe they're using LVDS type technology? Not sure what CSI/DSI specifies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    not sure myself, but the schematics show what appears to be three sets of differential pairs.  You might expect more problems with the I2C over a distance, but they're using fairly low value pullups, so probably ok unless it's running at high speeds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    That's very cool. So, Thomas, in that case, normal ribbon may be fine but it's an experiment, or something like Ethernet cable type wiring could be used in theory too, but that's an experiment too because the impedance might not match. And as Selsinork says, your limit may end up being the I2C control signals, unless it's a slow speed.