Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum got my raspberry Pi and what next?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 713 subscribers
  • Views 3548 views
  • Users 0 members are here
  • raspberry_pi
Related

got my raspberry Pi and what next?

hokelvin66
hokelvin66 over 13 years ago

i juz get my raspberry pi and a 4GB raspbeey Pi SD card with debian OS.However where should i start,since i am new here image.thx

  • Sign in to reply
  • Cancel
Parents
  • dwinhold
    dwinhold over 13 years ago

    I just received my second one today just to use as a media player. I just finished setting it up with Raspbmc, I have been using XBMC through an Apple TV 2. I figured this was a inexpesive way to have another player downstairs. It runs very well on the PI and so far am quite happy with it. Takes a bit setting up, but that is half the fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 13 years ago in reply to dwinhold

    I have a similar set up, except it uses the Squeezebox media center instead of XBMC.  I have SqueezeSlave installed on the RPi and control it from the web interface on the Squeezebox media server.  It makes a nice $40 replacement for the $300 radio that wore out years ago.

     

    My first RPi is still gonig strong.  It's running an internal DNS server for the house, a WOL gateway, Munin, and Bitlbee.  I think that, by using the WOL feature to wake up the house server only when it's needed, the dollar savings for electricity will more than offset the initial cost of the RPi.

     

    My next project is to add a ZWave interface to the RPi (search Google for RaZBerry) and seeing how well it works with the various modules offered at the local Lowes Hardware.  I'll have to add a Zigbee interface to play with Lowes' sensors.

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • groaker
    groaker over 13 years ago in reply to packetgeek

    Tim,

     

    I would be interested in hearing about adding the ZWave interface to the RPi should you decide to do this. TIA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 13 years ago in reply to groaker

    Michael,

     

    I've ordered the RazBerry interface.  Should be in some time this week (hopefully before the 4-day weekend).  Will keep you posted.

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to packetgeek

    did tim use enough acronyms and tech jargon to lose all of us beginners,,, makes me throw up image  just kidding guys,, but please spell out some of the acronyms

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 13 years ago in reply to e14 Contributor

    My apologies, what you rceived above was a mix of network geek, hardware geek, and Internet speak.  Happens at work also (someone stuck a sign on the outside of my cube: "WARNING!  Occupant communicates primarily via acronym!")    Further apologies as the list is a bit self-referential.

     

    Bitlbee - A program capabile of concurrently bridging multiple IRC and Jabber servers.

    DNS - Domain Name Service

    GUI - Graphical User Interface

    Munin - A program which gathers various system metrics and presents those metrics via graphs.

    RaZBerry - A ZWave enabled daughter board for the RPi.

    RPi - Raspberry Pi

    Squeezebox - Logitech used to sell what they called a SqueezeBox (think Internet radio).  It was the (hardware) client end that connected to a media server (called the Squeezebox Media Center) that you installed on your computer.  Had a built-in speaker, a volume knob, and a couple buttons.  Could connect to the network via wireless or wired connection.

    SqueezeSlave - A headless (no GUI) software-only client for Squeezebox.   There was also a GUI-enabled version called SoftSqueeze.

    WOL - Wake on LAN.  For certain computers, if configured properly, you can turn them on from the network by sending it a "magic packet". (Note: "magic packet" is the accepted term for the packet.)

    Zigbee - A low power, low bandwidth wireless technology used primarily in sensor networks.

    ZWave - A low power, low bandwidth wireless technology used primarily in home automation.

     

    If I've missed any, yell.

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • packetgeek
    packetgeek over 13 years ago in reply to e14 Contributor

    My apologies, what you rceived above was a mix of network geek, hardware geek, and Internet speak.  Happens at work also (someone stuck a sign on the outside of my cube: "WARNING!  Occupant communicates primarily via acronym!")    Further apologies as the list is a bit self-referential.

     

    Bitlbee - A program capabile of concurrently bridging multiple IRC and Jabber servers.

    DNS - Domain Name Service

    GUI - Graphical User Interface

    Munin - A program which gathers various system metrics and presents those metrics via graphs.

    RaZBerry - A ZWave enabled daughter board for the RPi.

    RPi - Raspberry Pi

    Squeezebox - Logitech used to sell what they called a SqueezeBox (think Internet radio).  It was the (hardware) client end that connected to a media server (called the Squeezebox Media Center) that you installed on your computer.  Had a built-in speaker, a volume knob, and a couple buttons.  Could connect to the network via wireless or wired connection.

    SqueezeSlave - A headless (no GUI) software-only client for Squeezebox.   There was also a GUI-enabled version called SoftSqueeze.

    WOL - Wake on LAN.  For certain computers, if configured properly, you can turn them on from the network by sending it a "magic packet". (Note: "magic packet" is the accepted term for the packet.)

    Zigbee - A low power, low bandwidth wireless technology used primarily in sensor networks.

    ZWave - A low power, low bandwidth wireless technology used primarily in home automation.

     

    If I've missed any, yell.

     

    - Tim