Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum how to hook it all up?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 707 subscribers
  • Views 1131 views
  • Users 0 members are here
  • raspberry_pi
Related

how to hook it all up?

e14 Contributor
e14 Contributor over 13 years ago

hi all,

 

I am leaning toword the Model A but I still have some questions for which I doesn't see any answers.

 

1. what can a person not do with 256M of ram that a person with 512M of ram can do?

 

2. is it possible to connect a keyboard, mouse, monitor, ethernet, and hard drive to a Model A?

    with or without a hub?

 

3. is there a faster/more expensive version say with a quad core cpu/more ram in raspberry's future?

 

thanks to all,

charles.......

  • Sign in to reply
  • Cancel
Parents
  • wallarug
    wallarug over 13 years ago

    1.  More ram means you can have more demanding applicatons running.  Such as games, 3D modelling, etc. It also gives you more speed in general because you are not writing to the swap file as much.

     

    2. No,  You will need a Model B for ethernet and connecting more than one USB device.

     

    3. No, the model B is the highest model avaiable ($10 more than Model A - there's your more expensive one image).

     

    If you want general setup information see this link:  http://www.raspberrypi.org/quick-start-guide

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to wallarug

    thanks for the response,

     

    I was wodering if I get a usb hub with 7 ports and I hooked it up to the one usb port on the pi Model A, couldn't I just hook the rest of the usb stuff up to the hub and have it all work?  Has anyone even thought of this or tried it?

     

    yes I know the price of the hubs.

     

    thanks,

    charles......

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    charles shultz jr wrote:

     

    I was wodering if I get a usb hub with 7 ports and I hooked it up to the one usb port on the pi Model A, couldn't I just hook the rest of the usb stuff up to the hub and have it all work?  Has anyone even thought of this or tried it?

    Yes, that should work assuming that the hub has an external power jack with a good 5V supply.  The hub's upstream cable connects to RasPi model A's single full-size USB A port.  If the 7-port hub back-powers the upstream cable (which it's not supposed to do, but many hubs do it anyway) then the upstream cable can power your RasPi.  Otherwise, you can usually connect a USB A male to Micro USB B male cable between a one of the hub's 7 downstream ports and RasPi's power jack.  This way you only need a single power supply for everything.

     

    The USB cable powering RasPi should be as short as possible.  You can actually get a sizeable voltage drop across some Micro USB cables, in some cases enough to prevent RasPi from working reliably.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 13 years ago in reply to e14 Contributor

    charles shultz jr wrote:

     

    I was wodering if I get a usb hub with 7 ports and I hooked it up to the one usb port on the pi Model A, couldn't I just hook the rest of the usb stuff up to the hub and have it all work?  Has anyone even thought of this or tried it?

    Yes, that should work assuming that the hub has an external power jack with a good 5V supply.  The hub's upstream cable connects to RasPi model A's single full-size USB A port.  If the 7-port hub back-powers the upstream cable (which it's not supposed to do, but many hubs do it anyway) then the upstream cable can power your RasPi.  Otherwise, you can usually connect a USB A male to Micro USB B male cable between a one of the hub's 7 downstream ports and RasPi's power jack.  This way you only need a single power supply for everything.

     

    The USB cable powering RasPi should be as short as possible.  You can actually get a sizeable voltage drop across some Micro USB cables, in some cases enough to prevent RasPi from working reliably.