Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum UART connections on Rpi GPIO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 1119 views
  • Users 0 members are here
  • research
  • helpme
  • element14
  • raspberry_pi
Related

UART connections on Rpi GPIO

tabarus12
tabarus12 over 13 years ago

Hi, does anyone know if the UART tx and rx pins can be used to connect usb devices directli to the GPIO connection of the Rpi?

Or can it be used to connect the pin0 and pin1 of the arduino as a direct serial link to the arduino?.

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 13 years ago

    Hi Omar,

     

    As I understand, the traditional Arduino uses 5V logic signals (whereas the Arduino Due uses 3.3V I believe), and the RPI uses 3.3V levels. You could connect the UART pins together across the two boards, but only if they are using the same logic levels. Otherwise, you need some level converter, something like this, powered from 3.3V.  (It is a quad NAND gate ic, you can tie the inputs together per gate, and tie the unused gate inputs to 0V). It is surface mount, but is the large SOIC package which is easy to solder.

     

    EDIT: ugh, sorry, you need something like this, not NAND, which will invert your logic (unless you chain them). I'm just so used to using NAND gates for everything..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • guzunty
    guzunty over 13 years ago

    Hi Omar,

     

    USB protocols are much more sophisticated than simple serial links. They have a hardware and a software component, and so you cannot connect the rx/tx lines directly to USB.

     

    What people do instead is to use something like this : http://www.adafruit.com/products/954

     

    As Shabaz said, you can only connect Arduino's directly to the Pi serial lines if the Arduino is running at 3.3v. This is possible, there's one on the Gertboard. However, you then can't run the Arduino at its full speed. For that reason, most off the shelf Arduinos are 5v based, which means you must use an interface chip. This one can do much more than interfacing to Arduinos: https://github.com/Guzunty/Pi/wiki. Disclosure: I curate this site.

     

    HTH,

     

    Derek

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to guzunty

    Yes: http://www.panu.it/raspand232/


    Alberto

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mgt6910
    mgt6910 over 13 years ago in reply to e14 Contributor

    My Firefox Browser has informed me that the certificates of this site can not be trusted.  I'll pass on that then, thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mgt6910

    I used the wrong protocol, post corrected!

    TX.

     

    Alberto