Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Sleepy Pi - A Sleep mode and Arduino I/O board. A Call For Volunteers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 708 subscribers
  • Views 3607 views
  • Users 0 members are here
  • pi
  • raspberry-pi
  • sleepy
  • add-on
Related

Sleepy Pi - A Sleep mode and Arduino I/O board. A Call For Volunteers

fuffkin
fuffkin over 13 years ago

I’ve been testing some of my Sleepy Pi prototype boards and am just about to order a number of next revision boards.

 

I’d love to give out some of this next batch of boards to the community to test out.

 

I actually designed this as an add-on to a humane Mouse-trap. These are all well and good, but if you don't check them every day, the poor mouse still snuffs it.  The idea of the Sleepy Pi is that it'll implement a "Wake-n-mouse" (as opposed to Wake-on-lan image) and take a photo of the captive mouse and either tweet or email it to me.

 

In terms of functionality the Sleepy Pi is essentially a Smart Power Management board for the Raspberry Pi that includes a low power Arduino that stays powered when the Raspberry Pi is off. In this way it can reduce the overall power used by the RPi, particularly when powered from batteries in applications where the RPi doesn’t need to be on all the time. You can think of it as adding a “Sleep” mode to the Raspberry Pi, because the Arduino can periodically wake the  RPi up to perform a task and then put it back to sleep. As a side benefit you also get some Arduino I/O to play with, like Analogue Inputs and PWM’s.


Key functions:

  • Reduce the effective Power consumption of the Raspberry Pi
  • Power directly from batteries up to 17V
  • Adds Arduino I/O to the Raspberry Pi such as Analogue In or PWM
  • Break out the Raspberry Pi GPIO & Arduino I/O to screw terminals
  • Prototyping area and expansion headers for daughter boards
  • Power button for manual switch on/off
  • “Wake” or “Sleep” in response to events or triggers such as:
    • Analogue value crosses a threshold
    • Digital input changes
    • Specific time to “wake” via Real-time Clock

 

Is this something people could use? Can you think of an applications you'd use one for?

 

I would love to hear any feedback. You can contact me either through the forum or on my blog at http:www.spellfoundry.com

 

Jon

  • Sign in to reply
  • Cancel
Parents
  • Nate1616
    Nate1616 over 13 years ago

    Jon

    I think this would be a great product.  I know off the top of my head one use i would use this for.  Being from Wisconsin and huge into hunting every year around late July we start to put out scout cameras to track the whitetails to tell us how many, what size and when they are moving on the property but having 100s of acres to walk around and swap out the sd card just takes forever.  What i want to do is attach a Pi to each camera and have it transmit all the pictures to 1 central station located in the cabin.  Now this transmission only has to be every 2 weeks or so, so this product would work great to turn on the pi and push what needs to be pushed then shut itself back off.  If your looking to have someone to test this i would be more than happy.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Nate1616
    Nate1616 over 13 years ago

    Jon

    I think this would be a great product.  I know off the top of my head one use i would use this for.  Being from Wisconsin and huge into hunting every year around late July we start to put out scout cameras to track the whitetails to tell us how many, what size and when they are moving on the property but having 100s of acres to walk around and swap out the sd card just takes forever.  What i want to do is attach a Pi to each camera and have it transmit all the pictures to 1 central station located in the cabin.  Now this transmission only has to be every 2 weeks or so, so this product would work great to turn on the pi and push what needs to be pushed then shut itself back off.  If your looking to have someone to test this i would be more than happy.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fuffkin
    fuffkin over 13 years ago in reply to Nate1616

    Hi Nate,

     

    Thanks for sharing that application, I love all the wildlife applications that are coming out. I started life as a Biologist, which led me to in a very roundabout route to Machine Vision & engineering. Anything that combines cameras with PI's and wildlife gets my vote (ok, even if you go and shoot them later image)

     

    I think the Sleepy Pi could definately be pressed into service here and I'll gladly send you one to test when they're ready.

     

    Jon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 13 years ago in reply to fuffkin

    LOL Jon.  Dont worry we are not out there just shooting anything.  We do deer management which means we try to keep a 1:4 ratio of bucks to doe and the bucks have to score at least 140 inches to shoot.  Let me tell you this has shown some pretty impressive results.  Its not uncommon now to shoot a buck that scores at least 160 inches.

     

    Nate