Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Sleepy Pi - A Sleep mode and Arduino I/O board. A Call For Volunteers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 708 subscribers
  • Views 3609 views
  • Users 0 members are here
  • pi
  • raspberry-pi
  • sleepy
  • add-on
Related

Sleepy Pi - A Sleep mode and Arduino I/O board. A Call For Volunteers

fuffkin
fuffkin over 13 years ago

I’ve been testing some of my Sleepy Pi prototype boards and am just about to order a number of next revision boards.

 

I’d love to give out some of this next batch of boards to the community to test out.

 

I actually designed this as an add-on to a humane Mouse-trap. These are all well and good, but if you don't check them every day, the poor mouse still snuffs it.  The idea of the Sleepy Pi is that it'll implement a "Wake-n-mouse" (as opposed to Wake-on-lan image) and take a photo of the captive mouse and either tweet or email it to me.

 

In terms of functionality the Sleepy Pi is essentially a Smart Power Management board for the Raspberry Pi that includes a low power Arduino that stays powered when the Raspberry Pi is off. In this way it can reduce the overall power used by the RPi, particularly when powered from batteries in applications where the RPi doesn’t need to be on all the time. You can think of it as adding a “Sleep” mode to the Raspberry Pi, because the Arduino can periodically wake the  RPi up to perform a task and then put it back to sleep. As a side benefit you also get some Arduino I/O to play with, like Analogue Inputs and PWM’s.


Key functions:

  • Reduce the effective Power consumption of the Raspberry Pi
  • Power directly from batteries up to 17V
  • Adds Arduino I/O to the Raspberry Pi such as Analogue In or PWM
  • Break out the Raspberry Pi GPIO & Arduino I/O to screw terminals
  • Prototyping area and expansion headers for daughter boards
  • Power button for manual switch on/off
  • “Wake” or “Sleep” in response to events or triggers such as:
    • Analogue value crosses a threshold
    • Digital input changes
    • Specific time to “wake” via Real-time Clock

 

Is this something people could use? Can you think of an applications you'd use one for?

 

I would love to hear any feedback. You can contact me either through the forum or on my blog at http:www.spellfoundry.com

 

Jon

  • Sign in to reply
  • Cancel
Parents
  • Nate1616
    Nate1616 over 13 years ago

    Hey Jonathan

    Just checking back in to see if you have any of these ready for beta testers.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fuffkin
    fuffkin over 13 years ago in reply to Nate1616

    Nate,

     

    You're absolutely right, about time for an update:

     

    The new boards are in and I've build up a couple for commissioning. I'm about half-way though this at the moment and so far no issues. If the other 50% also presents no major problems, I should be ready for a full update early next week, which hopefully will be kicking off the beta build and I can let you have some clearer dates then.

     

    Jon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fuffkin
    fuffkin over 13 years ago in reply to Nate1616

    Nate,

     

    You're absolutely right, about time for an update:

     

    The new boards are in and I've build up a couple for commissioning. I'm about half-way though this at the moment and so far no issues. If the other 50% also presents no major problems, I should be ready for a full update early next week, which hopefully will be kicking off the beta build and I can let you have some clearer dates then.

     

    Jon