Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Ethernet Causes Mouse Problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 708 subscribers
  • Views 1883 views
  • Users 0 members are here
  • x
  • bottom
  • ethernet
  • b
  • raspberry_pi
  • stick
  • wireless
  • mouse
Related

Ethernet Causes Mouse Problems

jreeve17
jreeve17 over 13 years ago

Hello, I have just purchased the Raspberry Pi Model B and have found a problem. Whenever I plug the Ethernet Cord in. The mouse (in x) drops to the bottom of the screen. Also, and keys i press become stuck and keep repeating untill I press another. Without the Ethernet cable, however the Pi works fine. I have tired reinstalling the  wheezy and different mice, but nothing works. The Keyboard also works fine, as I have been using it with my laptop with no problem.

I am using the Rasbian Wheezy with the GE Multimedia wireless keyboard and mouse.

How would I be able to fix or prevent this problem from happening?

Thanks in advance for any help you can give me.

 

Update: This problem is now happening even without the Ethernet cable plugged in. I have no idea why this is happening and still need help.

  • Sign in to reply
  • Cancel
Parents
  • jreeve17
    jreeve17 over 13 years ago

    @ John Beetem I am pretty sure that this is not a power issue as I am using a USB wall plug outputing 5V 1A. Could this be too much power?

    Also, you mentioned that one of my chips or crystals could be bad. Would getting a new Pi help solve this problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jreeve17
    jreeve17 over 13 years ago

    @ John Beetem I am pretty sure that this is not a power issue as I am using a USB wall plug outputing 5V 1A. Could this be too much power?

    Also, you mentioned that one of my chips or crystals could be bad. Would getting a new Pi help solve this problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to jreeve17

    Hi Reeve,

     

    It sounds like the symptom could be caused by one of several things. The problem is, replacing the board (i.e. if you think the crystal or chip is faulty) still won't help if the keyboard is not supported.

    Maybe try the easiest things first, such as trying a new keyboard if you have access to one, use a hub if it is wireless, and trying a different power supply (5V 1A is fine, but some high quality one is needed).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to jreeve17

    j reeve wrote:

     

    @ John Beetem I am pretty sure that this is not a power issue as I am using a USB wall plug outputing 5V 1A. Could this be too much power?

    Also, you mentioned that one of my chips or crystals could be bad. Would getting a new Pi help solve this problem?

    1A is not too much power.  5V at 1A means that the power supply can deliver up to 1A and is happy to deliver less current while maintaining 5V.

     

    The problem with RasPi power is that it has to go through a Micro USB cable and then through polyfuse F3 before it can be measured at TP1 and TP2.  Some micro USB cables have very thin conductors and you get a sizeable voltage drop.  Some F3 polyfuses are out of spec and cause an excessive voltage drop.  So if you have a multimeter or voltmeter, it's pretty easy to check that the voltage between TP1 and TP2 is 4.8V to 5.2V.  Iffy power can cause so many different symptoms that it's good to rule it out.

     

    If the LAN9512 chip or crystal is bad it's time for an RMA IMO.  Usually it's not the chip itself, but rather a bad solder joint, so some people who enjoy doing this sort of thing have reheated the X1 connections and made X1 work.  Everyone else should have the board replaced so that RasPi can improve the process.  I don't know how common the X1 problem is nowadays -- it was pretty rare even when RasPi was first being shipped.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jreeve17

    Would getting a new Pi help solve this problem?

     

    Probably not.  The problem is most likely that the RPi's USB system does not

    work well with certain wireless keyboards.  If you google for site:raspberrypi.org

    mouse bottom of screen, you will find a number of threads without solutions.

     

    If you are considering exchanging it, you might want to consider

    exchanging it for a Beaglebone Black, which as far as I know works

    fine with wireless keyboards.  It doesn't do 1080p video decode,

    but other than that, it is generally considered to be a better value

    than the RPi.