Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it possible to add a disk drive to a RPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 706 subscribers
  • Views 887 views
  • Users 0 members are here
  • raspberry_pi
Related

Is it possible to add a disk drive to a RPi

colnelb
colnelb over 13 years ago

I would like to add a 300GB USB disk drive to my RPi.  I have the latest download of the Debian OS for my RPi.  I have attached the disk drive to a USB hub that I have on the RPi.  Looking at the log messages, I see the message that the system has identified the drive on USB 1-1.3.4.3, but in never seems to get beyond that.  Are there any suggestions?  I would like to be able to do a permanant mount of this drive.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    It's difficult to do a permanent mount of what is essentially a removeable, hot-pluggable, device. You can try the following though

     

    # blkid

    /dev/sda1: UUID="898ee85d-ee12-4ab1-af0b-dece508ba70a" TYPE="jfs"

     

    then edit /etc/fstab and add a line like the following

    /dev/disk/by-uuid/898ee85d-ee12-4ab1-af0b-dece508ba70a    /data     jfs     defaults     0     1

     

    where /data is the mountpoint and needs to exist as an empty directory. Make sure the file ends with a blank line.

     

    Whether this is automatically mounted for you on boot depends somewhat on whether the disk has spun up and the usb subsystem has detected it before the boot sequence has tried to mount devices from fstab.  If it doesn't mount automatically, you can simply type 'mount /data' later to mount it.

    If you reformat, repartition, change the filesystem type, then it's a good bet that the uuid will be re-written and you'll need to update the line in fstab.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    It's difficult to do a permanent mount of what is essentially a removeable, hot-pluggable, device. You can try the following though

     

    # blkid

    /dev/sda1: UUID="898ee85d-ee12-4ab1-af0b-dece508ba70a" TYPE="jfs"

     

    then edit /etc/fstab and add a line like the following

    /dev/disk/by-uuid/898ee85d-ee12-4ab1-af0b-dece508ba70a    /data     jfs     defaults     0     1

     

    where /data is the mountpoint and needs to exist as an empty directory. Make sure the file ends with a blank line.

     

    Whether this is automatically mounted for you on boot depends somewhat on whether the disk has spun up and the usb subsystem has detected it before the boot sequence has tried to mount devices from fstab.  If it doesn't mount automatically, you can simply type 'mount /data' later to mount it.

    If you reformat, repartition, change the filesystem type, then it's a good bet that the uuid will be re-written and you'll need to update the line in fstab.