Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is it possible to add a disk drive to a RPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 706 subscribers
  • Views 885 views
  • Users 0 members are here
  • raspberry_pi
Related

Is it possible to add a disk drive to a RPi

colnelb
colnelb over 13 years ago

I would like to add a 300GB USB disk drive to my RPi.  I have the latest download of the Debian OS for my RPi.  I have attached the disk drive to a USB hub that I have on the RPi.  Looking at the log messages, I see the message that the system has identified the drive on USB 1-1.3.4.3, but in never seems to get beyond that.  Are there any suggestions?  I would like to be able to do a permanant mount of this drive.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I've never had to do the UUID that Selsinork is suggesting and my Pi does the mount at boot just fine of a usb drive.

     

    Quick questions:

        Are you trying to power this drive through the Pi's USB ports? 

        You say latest version of Debian, but is that actually Raspbian?  I ask because they seem to call debian the soft-float version and Rasbpian the hard float version (the hard float version makes use of a built in device on the SoC to get better performance)

        What is the file format of the drive

     

    The ultimate answer is to look into fstab.  Even if it's seeing the drive, it won't mount it unless you tell it to make it accesible in a specific location as Selsinork said. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The UUID piece is mainly so that, in theory, you always get the same device mounted in the same place regardless of device detection order. If you use /dev/sda1 and inadvertently leave a usb memory key attached then there's a chance that the key gets detected first, is assigned /dev/sda1 and gets mounted instead of the drive you expected.

    If you only ever connect this one drive, you're safe using /dev/sda1, but the nature of hot-pluggable busses means that's unlikely. Especially when USB is effectively the only expansion bus on the board.

     

    I'm not a fan of the disk-by-id & disk-by-uuid methods as they rely on data that's not guaranteed to be unique (clone your disk using dd and the clone has the same uuid since it's written to the disk) however they're no worse than many other methods.

    In a lot of ways I prefer LVM where you can use /dev/mapper/volumename, but LVM is overkill for a single volume on a single disk.

     

    The other way would be to use nfs and mount some filesystem exported from elsewhere on the network, however my relatively untouched Raspbian image doesn't seem to mount nfs from fstab by default.

     

    Even if it's seeing the drive, it won't mount it unless you tell it to make it accesible in a specific location as Selsinork said. 

    The exception to that is that often when you boot to a desktop environment they tend to run some process in the background that checks for new storage devices, mounts them under /media, and then pops up an icon on the desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    The UUID piece is mainly so that, in theory, you always get the same device mounted in the same place regardless of device detection order. If you use /dev/sda1 and inadvertently leave a usb memory key attached then there's a chance that the key gets detected first, is assigned /dev/sda1 and gets mounted instead of the drive you expected.

    If you only ever connect this one drive, you're safe using /dev/sda1, but the nature of hot-pluggable busses means that's unlikely. Especially when USB is effectively the only expansion bus on the board.

     

    I'm not a fan of the disk-by-id & disk-by-uuid methods as they rely on data that's not guaranteed to be unique (clone your disk using dd and the clone has the same uuid since it's written to the disk) however they're no worse than many other methods.

    In a lot of ways I prefer LVM where you can use /dev/mapper/volumename, but LVM is overkill for a single volume on a single disk.

     

    The other way would be to use nfs and mount some filesystem exported from elsewhere on the network, however my relatively untouched Raspbian image doesn't seem to mount nfs from fstab by default.

     

    Even if it's seeing the drive, it won't mount it unless you tell it to make it accesible in a specific location as Selsinork said. 

    The exception to that is that often when you boot to a desktop environment they tend to run some process in the background that checks for new storage devices, mounts them under /media, and then pops up an icon on the desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    The UUID piece is mainly so that, in theory, you always get the same device mounted in the same place regardless of device detection order. If you use /dev/sda1 and inadvertently leave a usb memory key attached then there's a chance that the key gets detected first, is assigned /dev/sda1 and gets mounted instead of the drive you expected.

    If you only ever connect this one drive, you're safe using /dev/sda1, but the nature of hot-pluggable busses means that's unlikely. Especially when USB is effectively the only expansion bus on the board.

    Very true, I've only worried about a single USB device on the Pi so I haven't had to worry about things like that.

     

    selsinork wrote:

     

    Even if it's seeing the drive, it won't mount it unless you tell it to make it accesible in a specific location as Selsinork said. 

    The exception to that is that often when you boot to a desktop environment they tend to run some process in the background that checks for new storage devices, mounts them under /media, and then pops up an icon on the desktop.

    Right again, I don't really like going into the gui on the pi so I didn't think about it, lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    I run Openelec on my RPi all the time and mount USB drives no problem as long as I do it on a powered hub...image