Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Touch Interface for the Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 1008 views
  • Users 0 members are here
Related

Touch Interface for the Raspberry Pi

techman1298
techman1298 over 13 years ago

Does anyone have any ideas to connect a Raspberry Pi to a 3.2" touchscreen display module from sainsmart? (or for any size touchscreen display for that matter)

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    Asuming you are talking about a four wire resistive touch panel, a good and quick way to deal with a touchscreen without too much hassle is to use a touchscreen controller like the TSC2004 form TI http://www.ti.com/product/tsc2004

     

    Given that you don't have ADC or extra GPIOs on the Rpi using an external controller with I2C is a good approach.

     

    -J

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • guzunty
    guzunty over 13 years ago in reply to jamodio

    You're talking about one of these, right?

     

    http://www.sainsmart.com/arduino-compatibles-1/lcd-module/sainsmart-3-2-tft-lcd-display-touch-panel-pcb-adapter-sd-slot-for-arduino-2560.html

     

    This module already has a touchscreen controller onboard, so no need for any additional controllers.

     

    Rodney, you're in luck. There has been a great deal of discussion and great work done on connecting these $16 displays. I will return and add more links, but the best site is:

     

    https://github.com/notro/fbtft/wiki

     

    These displays require more signals than the Raspberry Pi has available on the GPIO header, so you need to build a simple SPI interface. Notro describes how to build a discrete one, or you can use one of my Guzunty programmable IO devices:

     

    https://github.com/Guzunty/Pi/wiki

     

    I also made a daughter board which makes a nice neat 40 way ribbon cable connection. Here it is in action:

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • techman1298
    techman1298 over 13 years ago in reply to guzunty

    Thanks for the help Derek, i'll have it up and running soon image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • techman1298
    techman1298 over 13 years ago in reply to guzunty

    Thanks for the help Derek, i'll have it up and running soon image