Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Pi as developing board for ARM9 board and how to start my project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 705 subscribers
  • Views 2102 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi as developing board for ARM9 board and how to start my project

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I'm the new one here. My name is Ulrich in the outside world I'm a communication engineer in Finland. I'm having basic knowledge of Linux from doing school assignments which was always fun. Had also an ubuntu machine ones - unfortunately I had no time to play as much with as I wanted..

 

First I have to say that I'm sorry for asking here and taking your valueable time because I know that there are thousands of people asking for the same advice every day. I'm really willing to study myself, I just would like to have some guideliness for my project since I've no experience with embedded Linux. I read the book "Embedded Linux Development Using Eclipse" which was very good to get some basic information.

 

My project is based on an AT91SAM9G20 processor which should run an Angstrom Linux. The device should work as a fieldbus (KNX) coupler. There is going to be a webserver to see status and control the device. 

The reason why I am asking here, in the Raspberry Pi forum, is that I would like to know if I could use the Raspberry Pi as development board for this project since the final board is not available yet. Of course I couldn't connect it to the KNX but I think this is only a smaller part of the project anyways since I'm going to use ready made libraries there. I would like to know if I could easily transport the code (and knowledge) from Raspberry Pi to the final board. I guess this shouldn't be a problem if I could run the same OS on both of them?.. I have to admit that I'm a little bit confused and overwhelmed with all the different Linux software/plugins/packages etc. available.

Therefore I would appreciate it a lot if I could get some guideliness, or maybe a book recommondation, or maybe somebody could give me a link to similar project -  that would be great.

 

Thank you!

Ulrich

  • Sign in to reply
  • Cancel
Parents
  • jamodio
    jamodio over 13 years ago

    I'd suggest you setup a decent development environment in a Linux PC. You will have to use a cross compiler anyway, so the Raspberry Pi won't help you much, also compiling the kernel or other big chunks of code may take forever and put a lot of wear on the SD card or similar storage media.

     

    I don't have the link to the detailed instructions at hand but you can start looking at http://www.angstrom-distribution.org/building-angstrom

     

    My .02

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jamodio
    jamodio over 13 years ago

    I'd suggest you setup a decent development environment in a Linux PC. You will have to use a cross compiler anyway, so the Raspberry Pi won't help you much, also compiling the kernel or other big chunks of code may take forever and put a lot of wear on the SD card or similar storage media.

     

    I don't have the link to the detailed instructions at hand but you can start looking at http://www.angstrom-distribution.org/building-angstrom

     

    My .02

    Jorge

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jamodio

    Thank you Jorge! Yes, that might be the better way to go. I also read that several users are having trouble using angström with the BeagleBone Black.

    The link to the angström distribution I read before already. And again I'm a bit confused because I don't see any option there for a Linux PC processor - e.g. intel_x64. I will keep researching. 

     

    Best regards,

    Ulrich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    @Jorge: Right now I'm struggeling a bit with what you wrote. I thought for my task I don't need to modify the Linux kernel (regularly), or is there something I don't understand? I thought I just need to write an application for handling the fieldbus and setup the webserver..

     

    Ulrich