Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi GertBoard with DHT11 and EC/pH Transmitter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 503 views
  • Users 0 members are here
  • research
  • help
  • raspberry_pi
  • prototyping
  • raspberrypi
  • gertboard
Related

Raspberry Pi GertBoard with DHT11 and EC/pH Transmitter

e14 Contributor
e14 Contributor over 12 years ago

Hello there!!

 

 

I'm working on a prototype for enviromental monitoring.

 

I bought the last Raspberry Pi and the last GertBoard; i connected them with a home made ribbon cable (already tested with digital multimeter).

 

I need to get some data from two different enviroments: air and water.

 

Air monitoring:

- Temperature (°C)

- Humidity (RH %)

 

Water monitoring:

- PH (PH)

- EC (micro/S)

 

For the temperature and the humidity i bought the DHT11, a cheap but accurate sensor that i'm pretty sure you already know something about it.. Uses a single-wire serial interface.

 

For the water, i bought the two sensors conneted to a little unit.

This little unit gives me out two separate isolated analog signals: 0 - 5 Vdc.

 

Unit Specs.

""

Model A1005 EC/pH Transmitter with isolated outputs.

EC Range: 0-5 EC or 0-5000micro/S  . Error 2% .

pH Range: 0-14pH . Error .2%.

Outputs: EC 0-5vdc , pH 0-5vdc isolated.

Calibration: Trim pots for both EC and pH

""

 

 

Now the question: how should i connect all this parts together to get the best results?

 

 

Can you help me also to start writing the program?

I need to print the four values on the screen.

 

 

(maybe C is the best way, but if you have better suggestion i will be happy)

 

After this i will have to write some digital outputs, but i think it will be the easiest part..

 

Waiting answers.. Many thanks everybody for your help!

 

(I'm italian, sorry for my bad english!!!)

 

Federico

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    PS: Se volete lo riscrivo in italiano..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    PS: Se volete lo riscrivo in italiano..