Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiRack problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 677 subscribers
  • Views 2978 views
  • Users 0 members are here
  • piface_digital
  • raspberry_pi
  • raspberrypi
  • raspberryp-pi
  • pirack
  • piface
Related

PiRack problem

Former Member
Former Member over 12 years ago

I've got the PiRack yesterday and I've already tried to connect few things, including PiFace, LedBorg and ribbon cable to breadboard with temperature sensors connection. BUT. all of them worked without external power supply (both at once and separately tested), except for the PiFace! Even if only the PiFace is connected alone via the PiRack, it doesn't seem to be responding to Python commands...

To be on the safe side, I've swapped the jumpers from external to Pi power supply (no using external power at the moment at all), didn't touch the ISP jumpers at all (they are in default out-of-the-box positions.

Does the PiFace need an external power supply attached to the Pirack to be working?

  • Sign in to reply
  • Cancel
Parents
  • smythec
    smythec over 12 years ago

    Hi,

     

    We are also encountering problems with getting a PiFace to respond when connected via PiRack (we are using a PiRack to link 4 PiFace boards to the R-Pi).  We will be posting the solution in the next few days. The problem appears to be that the Python standard I/O module for R-Pi does not control the SPI lines of the GPIO interface. So you have to use the R-Pi GPIO module instead (this requires root access though).  The SPI CE lines have to be driven correctly - these lines are used to identifiy which PiFace is to be accessed (when using a PiRack PiFace is identified by the two jumprs J1, J2 settings on the PiFace. When the SPI CE lines are set correctly, data can be sent to the PiFace.

     

    We will post more next week when I hope we wil have written the Python code to get all of this to work.

     

    Colin S.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to smythec

    Thanks for a fast reply. I'm waiting for a more accessible solution and will try to make it work on my own. For now, should I change anyhow the J jumpers on the PiFace or the PiRack in order to make them work if I have only the Face on the Rack? And, should anything be added to the code to address it to the PiFace, like shown in the documentation examples?

    http://piface.github.io/pifacedigitalio/example.html#interrupts

    >>> p.digital_write(5, 1, 2) # writes pin5 on board2 high

     

    Message was edited by: Bartlomiej Bania

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 12 years ago in reply to smythec

    Thanks for a fast reply. I'm waiting for a more accessible solution and will try to make it work on my own. For now, should I change anyhow the J jumpers on the PiFace or the PiRack in order to make them work if I have only the Face on the Rack? And, should anything be added to the code to address it to the PiFace, like shown in the documentation examples?

    http://piface.github.io/pifacedigitalio/example.html#interrupts

    >>> p.digital_write(5, 1, 2) # writes pin5 on board2 high

     

    Message was edited by: Bartlomiej Bania