Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone interested in an Osborne 1 Raspberry Pi project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 707 subscribers
  • Views 988 views
  • Users 0 members are here
  • raspberry_pi
Related

Anyone interested in an Osborne 1 Raspberry Pi project?

cracksloth
cracksloth over 12 years ago

Do you guys remember the original portable computers - suitcase-style, "luggable" computers?  Osborne Computers made the first of them.  Anyway, I've got the 163rd one made up on Ebay:

http://cgi.ebay.com/ws/eBayISAPI.dll?ViewItem&item=111238132435

imageimage

The reason I am posting it here is because I always had hopes of doing integrate an Arduino or (more likely) a Raspberry Pi using the parallel port for a cool mix of old and new technology.  I thought it would be cool if whoever got it, had a similar point of view:

  • Cool text based home automation unit (using the parallel port with an Arduino or Raspberry Pi)
  • Use a Raspberry Pi, Google’s voice recognition API, and the Wolfram Alpha Python Interface to make a retro text version of Siri that looks like early artificial intelligence - kind of a steampunk home helper that you can ask questions to settle bar bets or check the weather
  • Freak people out at a presentation by hooking it up to projector and doing a minimalistic, text only "slideshow" (either using a "Screen Pac" and MBASIC or by hiding a Raspberry Pi inside)
  • Convert or swap the CRT to accept the composite out of a Raspberry Pi... monochrome goodness with unlimited possibility
  • Now that your Xbox 360 just got obsolete, time to hack it into a mobile version with room for controllers and the world's largest built-in chatpad
  • If you want to keep that monochrome feel, I played Atari 2600 games in monochrome and survived my childhood.  How about hacking an Atari into the case.  It would be a great little diversion to throw together and keep at a cabin, lodge, or man cave.  The Atari controller aesthetic would lend itself pretty well to the design of the case
  • Put it on display in the office of your startup - maybe have it rotate welcome messages to visitors.
  • Hack the 2 floppy drives to play dueling banjos...
  • screw a project, just have a piece of history

 

Anyone have any other cool ideas?

  • Sign in to reply
  • Cancel
Parents
  • myamiphil
    myamiphil over 12 years ago

    I also have an Osborne one sitting in my basement... Later version, upgraded with the double density and video out. Never got a HD for it. I was seriously considering the Rasbi until I discovered the UDOO quad. An A9 processor (quad core) and Arduino all on one board. Can run Linaro (Linux) or Android OS. Consider the UDOO to be 4 Rasbi's and Arduino all on one board, with HDMI, SATA HD, camera input, audio i/o, usb serial, CAN.

     

    The dream I have is to turn the Ozzy into a radio science platform. My interests are in radio and astronomy. Put the Udoo on a slide out rail to work on it during prototyping.... A LCD (touch screen) swings down over the center during normal op... I have a ULF NASA Inspire radio for natural RF (lightning and aural choruses...

    Also acquired an SDR usb dongle tv radio that can tune HF to UHF and beyond (2 GHz), got the dongle working under Windows and Mac so far. Linux is next. Radio astronomy has lots ofr amateurs under2 GHz.

     

    For the astronomy side Ill use Arduino stuff to control a telescope mount, focus, GPS etc.. The UDOO can run astronomy software and camera acquisition.

     

    Battery power, AC..maybe even solar charging for batteries. I can add a small s/w radio for signals under 2 MHz down to LF range. The Arduino can of course can be used for a weather station, motor control (servos for directional antennas, Telescope control.

     

    A dream machine for natural science activity. Ive held the Ozzy in sacred status all these years. It faithfully served me in the late 80's as the first one in my office to carry a "portable" computer for work.... But now its a perfect space for all kinds of ideas.

     

    Phil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • myamiphil
    myamiphil over 12 years ago

    I also have an Osborne one sitting in my basement... Later version, upgraded with the double density and video out. Never got a HD for it. I was seriously considering the Rasbi until I discovered the UDOO quad. An A9 processor (quad core) and Arduino all on one board. Can run Linaro (Linux) or Android OS. Consider the UDOO to be 4 Rasbi's and Arduino all on one board, with HDMI, SATA HD, camera input, audio i/o, usb serial, CAN.

     

    The dream I have is to turn the Ozzy into a radio science platform. My interests are in radio and astronomy. Put the Udoo on a slide out rail to work on it during prototyping.... A LCD (touch screen) swings down over the center during normal op... I have a ULF NASA Inspire radio for natural RF (lightning and aural choruses...

    Also acquired an SDR usb dongle tv radio that can tune HF to UHF and beyond (2 GHz), got the dongle working under Windows and Mac so far. Linux is next. Radio astronomy has lots ofr amateurs under2 GHz.

     

    For the astronomy side Ill use Arduino stuff to control a telescope mount, focus, GPS etc.. The UDOO can run astronomy software and camera acquisition.

     

    Battery power, AC..maybe even solar charging for batteries. I can add a small s/w radio for signals under 2 MHz down to LF range. The Arduino can of course can be used for a weather station, motor control (servos for directional antennas, Telescope control.

     

    A dream machine for natural science activity. Ive held the Ozzy in sacred status all these years. It faithfully served me in the late 80's as the first one in my office to carry a "portable" computer for work.... But now its a perfect space for all kinds of ideas.

     

    Phil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cracksloth
    cracksloth over 12 years ago in reply to myamiphil

    The UDOOs look really cool and I would love to fit one into a project if I can ever settle on what my next one should be...

    I love your idea - I had to laugh a little thinking of an Osborne with a touch screen!  There is so much room in those things that they can house pretty much anything you can dream up.

    So you carried one to work?  Is one arm longer now image