Raspberry Pi Forum I'd be giving the patents away...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 690 subscribers
  • Views 2501 views
  • Users 0 members are here
  • raspberry_pi
  • patents
Related

I'd be giving the patents away...

packetgeek
packetgeek over 12 years ago

A recent discussion, which appears to have (thankfully) been removed, involved a technology which was doubted by many.  Ignoring that it was inappropriate to advertise the thing an off-topic post, the thing that made me think that the tool was just more snake oil was the vendor's statement: "If I tell you everything you want to know,'I'd be giving the patents away!! and I cannot afford to do that."  If the author of that statement has a patent, then the information is already publicly available.  His statement makes me believe there is no patent and no actual working technology.

  • Sign in to reply
  • Cancel
Parents
  • R_Phoenix
    R_Phoenix over 12 years ago

    Thanks e14 for pulling those articles.

    I was able to read it when it was first posted and I had a good chuckle. While we have yet to understand all forms of energy exchange and the efficiency of most applications can be much improved on - there is no such thing as "free energy".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to R_Phoenix

    I believed that the Sun and Wind are "Free Energy"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    I've already explained the part that causes me to doubt the claims.  In

    short, the author's to justify secrecy to protect a patent.  It's not how

    patents work.  Add that to off-topic posting, promotion of a "technology"

    that has been rife with fraud for decades, the fees for trying out the

    dongle, and obfuscation of what is actually being done...  I use those as

    the basis of my opinion (I'm allowed to have one).  I didn't call for

    removal of the posts and I'm more than willing to perform any challenge as

    long as all fees are waived and I retain total control of my analysis and

    derivative content.

     

    MK, it's illogical to challenge anyone to provide any further analysis of

    the posts because there's very little "meat" in them.  I agree with another

    poster, where they'd thought that the dongle might be changing run-time

    settings in a Windows operating system, rather than harvesting energy from

    a CPU.

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to rew

    Roger,

     

    I concur.  One of the things taught in basic electrical engineering is that

    any energy conversion (mechanical to electrical, electrical to RF,

    electrical to chemical, etc.) is at best 80% efficient.  From there, it

    should be a simple power/time calculation to determine how much power needs

    to be harvested.  Keeping in mind that the claims require harvesting of

    "wasted" energy, that there's multiple energy conversion involved, and that

    the dongle doesn't harvest the heat from the CPU (where much of the energy

    consumed by the CPU ends up), the conversion process still remains suspect

    (in my opinion).

     

    -Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Of course you are allowed to have an opinion - no-one (as far as I know)  disputes that.

    What I was trying to point out is that it is better to discuss (and disprove) things rather than to pull posts.

    If the OP won't provide  a dongle for actual measurement it's hard to take his device at all seriously.

    I'm interested that many of the arguments presented against the device working rely on assertions rather than evidence or fact.

    For example - the device only has two connections, power and ground (which is clear from a photo) so it can't be affecting the laptop settings via USB.

     

    You suggest that there is some limit to conversion efficiency

     

    any energy conversion (mechanical to electrical, electrical to RF,

    electrical to chemical, etc.) is at best 80% efficient.

     

    but this just isn't true and there is no physical reason why it should be. (and in the spirit of scientific reasoning which I am defending, here is some evidence to back up my assertion : http://www.csiro.au/solutions/psz7)

     

    Just for the record I don't think, (on the basis of casual application of 2nd Law of Thermodynamics and some of the circumstantial evidence) that it will work.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • packetgeek
    packetgeek over 12 years ago in reply to michaelkellett

    Guessing: the comparison involves different loads on the motor (i.e.,

    comparing one output to the other).  My statement applied to conversions

    between different forms of energy.  I'll withhold any further comment on

    the topic as we're just chasing each others tails with this discussion.

    I'd rather get back to experimenting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to packetgeek

    Sometimes it's hard to let the other guy have the last word image

     

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    But motor efficiency (in the context of the link I provided) is mechanical power out/ electrical power in.

    Funny I was thinking the same thing.

     

    In the case of this device, it isn't converting energy from its electrical state, and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Test challenge

    I still haven't heard back, and obviously there would be no cost to the testers, otherwise its not fair.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to mcb1

    DC/DC is still from electrical to electrical; although applicable in the context of the product discussed, I think packetgeek meant conversion from one domain to the other.  Anyway, he's wrong as ThinGap claims 95% efficiency: http://www.thingap.com/efficiency-and-smoothness/ and the CSIRO motors have way more efficiency than 80%.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to mcb1

    mcb1 wrote:

    ... and I do know of DC to DC converts in the high 90's% of efficiency.

     

    Right. That's marketing-speak. In general DCDC converters convert at "around 80%" efficiency. Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency. The marketing guys jump on this number and prominently place it everywhere they can. In reality, count on 80% and let yourself be surprised if possible.

     

    The "80%" mentioned is a good ballpark figure. There are exceptions. Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

     

    On the other hand, going from chemical (gas) to mechanical power (moving car), you are lucky if you hit the 30%.

     

    As another example of how "ballpark figures" work I use "0.8" as the density of "organic materials". Wood, gasonline, etc. I know there are woods that are so dense that they sink (i.e. >1.0). But as a ballpark figure this 0.8 still works quite well. (e.g. when they say an airplane had XXX kg of fuel on board).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to rew

    Gas-powered central heating installations here in the Netherlands apparently achieve 107% efficiency according to the official efficiency-calculating-rules. If you WANT to go from electrical power to heat, that can easily be done with 100% efficiency.

    That's because in the official rules (when efficinecy was much, much lower) they thought that the heat going through the chimney was neglectabe..... Now that that heat loss is reduced, you get more than 100% efficiency. It's more an calculation / definition error. 107% efficiency would mean you'd be generating energy more heat than is available in caloric energy in the gas...

     

    Then when you sweep the output current along the whole range, at one point you may measure "above 90%" efficiency

    Yes. And when your application permits, you can design to be in that sweet spot. So it's a marketing-overused, but not a lie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 12 years ago in reply to vsluiter

    It's not the "heat going through the chimney" that they neglected in the definition at first.

     

    It's the energy that is contained in the water-vapour that goes up the chimney that they neglected. That can be recovered if you make sure the water condenses and you can leave the resulting water somewhere (a drain).

     

    If you build a heat-pump, powered either by gas or by electricity, you can get even higher efficiency figures, well above 100%.

     

     

    P.S; I fully agree with you to call the 107% situation a "definition error".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 12 years ago in reply to vsluiter

    It's not the "heat going through the chimney" that they neglected in the definition at first.

     

    It's the energy that is contained in the water-vapour that goes up the chimney that they neglected. That can be recovered if you make sure the water condenses and you can leave the resulting water somewhere (a drain).

     

    If you build a heat-pump, powered either by gas or by electricity, you can get even higher efficiency figures, well above 100%.

     

     

    P.S; I fully agree with you to call the 107% situation a "definition error".