Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Gpio problem Rpi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 678 subscribers
  • Views 1514 views
  • Users 0 members are here
  • raspberry_pi
Related

Gpio problem Rpi

Former Member
Former Member over 11 years ago

My raspberry pi 3v3 is not getting power (getting 1V when checked with multimeter) and other Gpio's are also not working properly i have checked with trouble shooting methods so power supply and polyfuse is proper what will be the problem anybody can help?

 

Thank you

  • Sign in to reply
  • Cancel
Parents
  • rew
    rew over 11 years ago

    On AVR processors, if you configure a pin as "input", setting the "output" bit will enable a "weak pullup". This is normally so weak that you wouldn't see a led light up. (it can be seen when you try and with an efficient led, but it's much weaker than you'd expect from a led).

     

    It works a bit differently on the BCM2835, but still it sounds as if you're just playing with the "weak pullup" instead of the output bit.

     

    Do you have a multimeter? Put a 220 ohm resistor (*) in series with your multimeter in "current" mode. Measure the current out of the GPIO pin. about 15mA is what we expect, 12-18 would be "expected". If you get say 60 micro A, that would be a "weak pullup" in action....

     

    The raspberry pi GPIO pins are 3.3V, so lighting a 3.6V white led is not going to work. What color led do you have and what does your supplier claim as the forward voltage?

     

    (*) I see you have a  270 ohm resistor. That'd be fine too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 11 years ago

    On AVR processors, if you configure a pin as "input", setting the "output" bit will enable a "weak pullup". This is normally so weak that you wouldn't see a led light up. (it can be seen when you try and with an efficient led, but it's much weaker than you'd expect from a led).

     

    It works a bit differently on the BCM2835, but still it sounds as if you're just playing with the "weak pullup" instead of the output bit.

     

    Do you have a multimeter? Put a 220 ohm resistor (*) in series with your multimeter in "current" mode. Measure the current out of the GPIO pin. about 15mA is what we expect, 12-18 would be "expected". If you get say 60 micro A, that would be a "weak pullup" in action....

     

    The raspberry pi GPIO pins are 3.3V, so lighting a 3.6V white led is not going to work. What color led do you have and what does your supplier claim as the forward voltage?

     

    (*) I see you have a  270 ohm resistor. That'd be fine too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to rew

    Pls understand that am telling about 3.3v Power pin am not getting power to that pin after a boot up but am getting 3.3v when didn't inserting memory card