Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PI Protection Guaranty!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 983 views
  • Users 0 members are here
  • pi
  • raspberry_pi
Related

PI Protection Guaranty!

e14 Contributor
e14 Contributor over 12 years ago

Si I recently fried my first Pi. I would be less heart broken if it wasnt because I actually had the nerve to snip a wire on a project board while everything was up and running. ( kick me) needless to say, metal scissors and microprocessors dont mix. Nevertheless, it gave me a great idea for driving DC motors and relays safely using ambient light sensors and LED's.

 

length of black rubber hose,

electrical tape

ambient light sensor radioshack 4-pack, 2.79

loose pack of LED's (anything but ultraviolet)

appropriate transistors and resistors to get the job done.

 

 

cut the hose to 1/2" and insert the light sensor in one end, and an LED in the other. Make sure no light is leaking in behind the light sensor  OR the LED.  Drive the LED with your Pi( pulse width works fine) and drive the transistor with the light sensor. Then kick yourself for not thinking of this sooner! (I did),

 

I've been using this all day, and it seems to be working fine, and there is no physical connection to my sloppy project board and my pi what so ever.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    the timing is a bit erratic, but there is no chance of bricking your pi, and for flipping motors n' relays, a little extra program effort is better than volt spikes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • iagorubio
    iagorubio over 12 years ago

    Kudos my dear Ray, you have just invented the optocoupler image

     

    Opto-isolator - Wikipedia, the free encyclopedia

    http://uk.farnell.com/jsp/search/browse.jsp?N=2031+203598&Ntk=gensearch&Ntt=optocoupler&Ntx=mode+matchallpartial

     

    Anyway next time check the net for flyback diodes or clamp diodes.

     

    It's the "flyback" what fries your Pi. Any inductive load, DC motors and relays, send back voltage spikes when the magnetic field on its coils collapses, That is called "flyback".

     

    You can drive that voltage spike safely back to the inductive load by connecting some diodes inverted between the plus and minus wires of your motor. As they are inverted - they point to the plus wire - they normally don't drive any voltage, but when the voltage spike comes back from the motor, the charge in the ground wire suddenly is greater than in the plus wire so they suddenly invert polarity and drive the spike back to the motor opening a loop.

     

    Look at this schematic and forget about the IC.

     

    http://www.elektrotekno.com/userpix/6181_l298_2.jpg

     

     

    All those diodes D1 to D8 you see connecting ground to motor wires and to +Vs are flyback diodes to protect the IC from spikes.

     

    The easiest way to use them is to buy some darlington transistor arrays - that in the other hand can also help you to drive relays and DC motors with higer voltages than your Pi can handle - with those diodes built in.

     

    MIC5800YN - MICREL SEMICONDUCTOR - DARLINGTON ARRAY 4 LATCHED, 5800 | Farnell UK

    https://www.google.es/search?q=darlington+array+with+clamp+diodes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to iagorubio

    There's a good article on flyback diodes at Wikipedia: http://en.wikipedia.org/wiki/Flyback_diode

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to iagorubio

    I am familiar with 'flyback' I did some fuel cell experiments back in the day, and encountered several free energy concepts that try to capture collapsing fields and convert them into usable energy. I think that is the key to zero point, but I'm not going to unlock it in front of my pc. I fried my pi when i snipped the power and shorted it out. rookie mistake. as for the optocoupler. too bad I did'nt invent it first or I would be rich! nevertheless, i 're-invented' it, so I will pat my own back!