Raspberry Pi Forum How do I right to a 556-ATMEGA48-20PU
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 685 subscribers
  • Views 854 views
  • Users 0 members are here
  • to
  • program
  • raspberry_pi
  • how
Related

How do I right to a 556-ATMEGA48-20PU

Former Member
Former Member over 12 years ago

Hello I have little active knowledge of electronics,I have always wanted to develop skills in this area.  I have set myself a task , Which I hoped was achievable when I set it but have come across one or two problems. My current goal is to use the indestructible link (Infrared Proximity Sensing Coffee Table Module & Color Changing Glowing Faucet) to create an interactive artwork for kids. I can get hold of the parts, and put them together, The programming looks to be correct. But I cannot work out how to get the programming onto the chip. What sort of equipment I would need ect ect. I suspect this is all basic stuff but as a fella with high school summer jobs as my experience I am struggling to find the answer for myself. Any help would be greatly appreciated. Kind regards, Phil   PS the chip is an

556-ATMEGA48-20PU

Atmel Microcontrollers (MCU)

4kB Flash 0.256kB

  • Sign in to reply
  • Cancel
Parents
  • iagorubio
    iagorubio over 12 years ago

    I agree with Bruce, pick up an arduino and try it.

     

    If you need help with the programming just ask here.

     

    Take into account that a Arduino board is just an ATmega chip on a development board so you can use that same program modified, if the board you get have enough i/o pins. You just need to translate the pins from the program you've got to the arduino pins.

     

    Those are the arduino Uno pin mappings http://arduino.cc/en/Hacking/PinMapping168

     

    The outer red ones are the labels on the arduino board, the inner black ones are the ATmega pin names. If you check the instructable source code you will see the ATmega pin names he is using.

     

    The programming environment you see in the instructable - avr gcc and programmers notepad - is included - but somewhat hidden in the tools directory- on the arduino windows SDK.

     

    It's a hard project to start with, but you can pick up an arduino go for it while learning a little more.

     

    Anyway, to program the ATmega directly I use my AVR Dragon with a  ZIP socket.

     

    Exactly the same programmer used in this instructable Help: An Absolute Beginner's Guide to 8-Bit AVR Programming-AVR Dragon : How to Prepare the AVR Dragon for AVR Programmi…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • iagorubio
    iagorubio over 12 years ago

    I agree with Bruce, pick up an arduino and try it.

     

    If you need help with the programming just ask here.

     

    Take into account that a Arduino board is just an ATmega chip on a development board so you can use that same program modified, if the board you get have enough i/o pins. You just need to translate the pins from the program you've got to the arduino pins.

     

    Those are the arduino Uno pin mappings http://arduino.cc/en/Hacking/PinMapping168

     

    The outer red ones are the labels on the arduino board, the inner black ones are the ATmega pin names. If you check the instructable source code you will see the ATmega pin names he is using.

     

    The programming environment you see in the instructable - avr gcc and programmers notepad - is included - but somewhat hidden in the tools directory- on the arduino windows SDK.

     

    It's a hard project to start with, but you can pick up an arduino go for it while learning a little more.

     

    Anyway, to program the ATmega directly I use my AVR Dragon with a  ZIP socket.

     

    Exactly the same programmer used in this instructable Help: An Absolute Beginner's Guide to 8-Bit AVR Programming-AVR Dragon : How to Prepare the AVR Dragon for AVR Programmi…