Raspberry Pi Forum Wolfson and MPD  working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 684 subscribers
  • Views 5175 views
  • Users 0 members are here
Related

Wolfson and MPD  working

superpat
superpat over 12 years ago

Hi,

 

I installed MPD onto the provided Wolfson Audio distribution, running it headless,  console via ssh.

 

I copied the provided demo flac files to the mpd music directory.

 

I ran alsamixer and wound up the digital i/p's and outputs.

 

controlling  MPD with the GMPC client on my LInux desktop

 

96Kbps flacs are playing  superbly, output  lineout  and into my desktop audio amp and speakers,

 

Next I will set mpd to get music from my NAS using nfs, which will be interesting, as this tends load the Pi system and  cause problems with the Pi and usb dacs!

 

cheers

 

 

P

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    Hello,

    I using Raspian + MPD + Wolfson audio card over NFS. I plugged the Lineout output on Hifi amplifier and it's working well except one thing : the volume control.

    I can't control volume with any Music Player clients.

    I think the mixer is not correctly configured but I don't know how I can configure it. Do you have any suggestions (tests or settings ) ?

     

    Thank you in advance !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago

    Hello,

    I using Raspian + MPD + Wolfson audio card over NFS. I plugged the Lineout output on Hifi amplifier and it's working well except one thing : the volume control.

    I can't control volume with any Music Player clients.

    I think the mixer is not correctly configured but I don't know how I can configure it. Do you have any suggestions (tests or settings ) ?

     

    Thank you in advance !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hi Alexis,

    I had the same problem. But I think I finally found the right setting to use the hardware mixer of the WM5102 with mpd. This is the important part of the mpd.conf:

    audio_output {
        type          "alsa"
        name          "Wolfson"
        device        "hw:0"
        mixer_type    "hardware"
        mixer_control "HPOUT2 Digital"
    }

    But be careful I'm not sure if this is fully correct and reduce the volume of your amp. Just in case ;-)

     

    If this matters: I use alsa-utils 1.0.28-1 and mpd 0.18.12-1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hello,

    Thank you twoflower.

    I can now control the volume through my favourite mpd client. However, It's difficult to adjust the volume without saturating my amplifier, because it seems that the volume scale is not linear but something almost exponential.

    Do you know if I can limit the upper volume value to avoid this behaviour ?