Raspberry Pi Forum Wolfson and MPD  working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 684 subscribers
  • Views 5178 views
  • Users 0 members are here
Related

Wolfson and MPD  working

superpat
superpat over 12 years ago

Hi,

 

I installed MPD onto the provided Wolfson Audio distribution, running it headless,  console via ssh.

 

I copied the provided demo flac files to the mpd music directory.

 

I ran alsamixer and wound up the digital i/p's and outputs.

 

controlling  MPD with the GMPC client on my LInux desktop

 

96Kbps flacs are playing  superbly, output  lineout  and into my desktop audio amp and speakers,

 

Next I will set mpd to get music from my NAS using nfs, which will be interesting, as this tends load the Pi system and  cause problems with the Pi and usb dacs!

 

cheers

 

 

P

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    I noticed that today too. The evening I found this configuration I was not trying this out in the sake of my neighbors sleep. So far I haven't found a fully working solution. Reducing the input levels of the mixer seems to help little:

    > amixer -Dhw:0 cset name='HPOUT2L Input 1 Volume' 10
    > amixer -Dhw:0 cset name='HPOUT2R Input 1 Volume' 10

    But the distortion stays there. I wish I would have a scope here to understand a little better what happens. And/Or some more time to read the 500+ pages datasheet of the WM5102.

     

    UPDATE: OK, I think I understand what's going on. According to the WM5102 datasheet all values above 0x80 (128) will amplify the input signal. That's what we want to avoid. This behavior seems to be true for most if not all volume knobs in the device. This might be useful in case you have low input signals. But in normal cases this will cause distortions. A solution might be to tell alsa (the mixer used by mpd) that the maximum value is not 0xBF (191) but 0x80 or a bit lower to avoid clipping. But so far I was not able to find the place to override the default. If I understand this right, alsa 'asks' the device about which knobs and values are valid. So there's no existing config file to tweak. But I'm sure there's a way to override stuff. One candidate is to create a alsactl_init but this seems to be not a 5 minute task to understand.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago

    I noticed that today too. The evening I found this configuration I was not trying this out in the sake of my neighbors sleep. So far I haven't found a fully working solution. Reducing the input levels of the mixer seems to help little:

    > amixer -Dhw:0 cset name='HPOUT2L Input 1 Volume' 10
    > amixer -Dhw:0 cset name='HPOUT2R Input 1 Volume' 10

    But the distortion stays there. I wish I would have a scope here to understand a little better what happens. And/Or some more time to read the 500+ pages datasheet of the WM5102.

     

    UPDATE: OK, I think I understand what's going on. According to the WM5102 datasheet all values above 0x80 (128) will amplify the input signal. That's what we want to avoid. This behavior seems to be true for most if not all volume knobs in the device. This might be useful in case you have low input signals. But in normal cases this will cause distortions. A solution might be to tell alsa (the mixer used by mpd) that the maximum value is not 0xBF (191) but 0x80 or a bit lower to avoid clipping. But so far I was not able to find the place to override the default. If I understand this right, alsa 'asks' the device about which knobs and values are valid. So there's no existing config file to tweak. But I'm sure there's a way to override stuff. One candidate is to create a alsactl_init but this seems to be not a 5 minute task to understand.